2021-05-14 11:38 AM
hi friends
i build a code with cubemx and i edited it too many times in all of them after 1 time conversion my code hanged. after all i can edit a code that countiniously works . i need to measure a fast analog signal in a specific time, for that reason i simulated that signal in a way that i produce a pwm signal and give it to a rc circuit and output is like a triangle wave.i what to sample in rise time or fall time by 7.2MSAMPLE/SEC speed in that time(2.5us and about 10 sample) . after 1 time i use HAL_ADCEx_MultiModeStart_DMA(&hadc1, (uint32_t*)num1, 10)
ten sample is almost true but it seen it is not in order, after that second time that program call
HAL_ADCEx_MultiModeStart_DMA(&hadc1, (uint32_t*)num1, 10) there is just 1 number in all of array and result is not true and repeated . i attach my code and pwm signal after rc filter.
what are my mistakes? why there is no clear datasheet about hal library ? and i search alot but i cant find a clear explain about multimode.DMAAccessMode = ADC_DMAACCESSMODE_1 ------ line
which mode i should use?
do have any good refrences?
please help -
thanks alot
2021-06-22 11:36 PM
Hello Akhan,
There is an example in the HAL library about the multimode : STM32756G_EVAL/Examples.../ADC/ADC_TripleModeInterleaved
Maybe It could be a good reference example for your application ?
Regards,
Simon
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.