2021-11-17 1:27 AM
Hi, last time I ported an Azure RTOS project there were only a handful of BSPs so I had to do some manual fiddling around to get it running on a nucleo board. Now that there is full support for H7 processors in the 2.0 package I'm wondering what the best steps to move a project over would be.
I imagine I can start a new project in CubeMX and then "import" the ioc file, generate the base project and then copy in the source code - but wondering if there is a cleaner way of doing it.
TIA, Oliver
Solved! Go to Solution.
2021-11-17 11:57 PM
Hi,
As you said you need to generate a new project for target board/MCU first then :
1-configure the HW IPs (GPIO, System clock, ETH, USB,,..)
2- Enable/Configure the components of Azure RTOS pack
3- Generate project and copy application source code from an existing example into your new project
2021-11-17 11:57 PM
Hi,
As you said you need to generate a new project for target board/MCU first then :
1-configure the HW IPs (GPIO, System clock, ETH, USB,,..)
2- Enable/Configure the components of Azure RTOS pack
3- Generate project and copy application source code from an existing example into your new project
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.