STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L4: HAL_MMC driver - get stuck in MMC_ReadExtCSD()

I'm using STM32L4A6 and it's SDMMC peripheral to communicate with an eMMC device.I found it occasionally get stuck in the MMC_InitCard() call. Further investigation shows it's stuck in the MMC_ReadExtCSD() call, where it utilizes a timeout value of 0...

CZ.4 by Associate II
  • 3300 Views
  • 4 replies
  • 0 kudos

Repeated start with HAL drivers on STM3273C

Hello, I am using the STM3273C board as an i2c slave. The master is requesting the data via repeated start.For this I am using the method HAL_I2C_Slave_Sequential_Transmit_IT. The problem is that the first byte after the restart is always 0xFF. The d...

AEsca.2 by Associate
  • 1062 Views
  • 1 replies
  • 0 kudos

Resolved! Creating bootloader for STM32F746GZ .

Hi guys.. I have to create a bootloader for the micro  STM32F746GZ . I have already an existing application for such a micro. I need to create the bootloader and then jumping from bootloader to the existing application. Any ideas about how to do it i...

SGasp.1 by Senior
  • 1250 Views
  • 1 replies
  • 0 kudos

HID - CDC Composite inf file on Windows 10

I am trying to learn about implementing a composite usb device. I have seen that Cube does not provide a ready solution for this and so I downloaded the USB FW library along with the examples. There is an example for a HID-CDC composite.I have seen t...

DRega.1 by Associate III
  • 9282 Views
  • 10 replies
  • 0 kudos

Resolved! MSC Class USB Device descriptor

Hello,I have setup the USB Device as MSC Class, connected to SD Card so once I connect to PC I can access to SD by Windows Explorer. It is shown as generic USB Device. How can I configure with a custom name descriptor?Thank you

lukin by Associate III
  • 1093 Views
  • 1 replies
  • 0 kudos

Looks like a silIcon bug in MAC Ethernet controller on STM32H753 MCU: unexpected IRQ execution after transmittion of 0x80000000 packets

Hi everybody. We're facing some issues with MAC Ethernet controller on STM32H753 MCU. Situation looks like a silicon bug: after transmitting of 2147483648 (0x80000000) packets over Ethernet the internal MAC controller in the specific circumstances st...

leshich-k by Associate II
  • 2312 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.