2019-08-08 7:10 AM
I've got a project in which I have to communicate by Ethernet (TCP) Nucleo-STM32F429ZI with PC. STM32 will be sending the data from sensor periodically. I'm using STM32CubeIDE with built in CubeMX. I've connected the STM32 and the PC with a crossed cable. I configured it without RTOS, only using LwIP in RAW API mode with static IP addresses. I’m calling the MX_LWIP_Process() function in while loop.
My problem is that I can't receive ping response from STM32 and I’m getting the “Destination Host Unreachable�? message. I've tried every configuration and advice I found on forums and it didn't work. I've tried to adapt my project configuration to that from the example for my board (LwIP_HTTP_Server_Netconn_RTOS which works and response) but it didn't work too.
As I'm debugging my project I can receive the ARP frame with request for IP address and I can see in debugger that the output frame is correct but as the whole payload is passed to "HAL_ETH_TransmitFrame" function, the output/response frame is gone, I can't see it in the Wireshark. I've checked the pinout configuration for the Ethernet peripheral and the configuration addresses. I really don't know what I’m missing.
I've got auto-negotiation enabled in ETH CubeMX and I've change the PHY address from default 1 to 0 and PHY Link down inturrupt from 0xB to 0x10 according to datasheet (I hope it's correct).
Below I pasted my configuration for Ethernet PHY (LAN8742A):
/* LAN8742A_PHY_ADDRESS Address*/
#define LAN8742A_PHY_ADDRESS 0U
/* PHY Reset delay these values are based on a 1 ms Systick interrupt*/
#define PHY_RESET_DELAY ((uint32_t)0x00000FFFU)
/* PHY Configuration delay */
#define PHY_CONFIG_DELAY ((uint32_t)0x00000FFFU)
#define PHY_READ_TO ((uint32_t)0x0000FFFFU)
#define PHY_WRITE_TO ((uint32_t)0x0000FFFFU)
/* Section 3: Common PHY Registers */
#define PHY_BCR ((uint16_t)0x00U) /*!< Transceiver Basic Control Register */
#define PHY_BSR ((uint16_t)0x01U) /*!< Transceiver Basic Status Register */
#define PHY_RESET ((uint16_t)0x8000U) /*!< PHY Reset */
#define PHY_LOOPBACK ((uint16_t)0x4000U) /*!< Select loop-back mode */
#define PHY_FULLDUPLEX_100M ((uint16_t)0x2100U) /*!< Set the full-duplex mode at 100 Mb/s */
#define PHY_HALFDUPLEX_100M ((uint16_t)0x2000U) /*!< Set the half-duplex mode at 100 Mb/s */
#define PHY_FULLDUPLEX_10M ((uint16_t)0x0100U) /*!< Set the full-duplex mode at 10 Mb/s */
#define PHY_HALFDUPLEX_10M ((uint16_t)0x0000U) /*!< Set the half-duplex mode at 10 Mb/s */
#define PHY_AUTONEGOTIATION ((uint16_t)0x1000U) /*!< Enable auto-negotiation function */
#define PHY_RESTART_AUTONEGOTIATION ((uint16_t)0x0200U) /*!< Restart auto-negotiation function */
#define PHY_POWERDOWN ((uint16_t)0x0800U) /*!< Select the power down mode */
#define PHY_ISOLATE ((uint16_t)0x0400U) /*!< Isolate PHY from MII */
#define PHY_AUTONEGO_COMPLETE ((uint16_t)0x0020U) /*!< Auto-Negotiation process completed */
#define PHY_LINKED_STATUS ((uint16_t)0x0004U) /*!< Valid link established */
#define PHY_JABBER_DETECTION ((uint16_t)0x0002U) /*!< Jabber condition detected */
/* Section 4: Extended PHY Registers */
#define PHY_SR ((uint16_t)0x1FU) /*!< PHY status register Offset */
#define PHY_SPEED_STATUS ((uint16_t)0x0004U) /*!< PHY Speed mask */
#define PHY_DUPLEX_STATUS ((uint16_t)0x0010U) /*!< PHY Duplex mask */
#define PHY_ISFR ((uint16_t)0x001DU) /*!< PHY Interrupt Source Flag register Offset */
#define PHY_ISFR_INT4 ((uint16_t)0x0010U) /*!< PHY Link down inturrupt */
My whole project is in the attachment. If you need any additional information about the setup please ask. Thank you very much for any help.
2020-10-19 12:36 PM
Hi Nukat,
Did ou solve your problem? I´ve just bought a nucleo-F429Zi board to implement a socket project. What do you think? can I use this board? Will it support ethernet communication?
Thanks,
Geraldo.
2022-06-29 4:56 AM
your problem might be in platform setting section of LWIP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.