2022-01-18 9:22 AM
Hello Everyone,
i am desperadely looking for help/guide on how to transfer data from a Windows PC to a controller using tcp / udp (via ethernet connection) and how to use the transferred data as an signed integer for some operations (for example setting some Output oft he controller). The transferred Data from the PC is only an intiger which ranges from -50 to 250. It doesnt matter if the controller has a fixed ip-adress or not. I have read some documents and guides regarding lwip and using webservers for the data transfer, but this isn’t what i am looking for.
Excample:
1. Connecting the controller with a PC via Ethernet
2. typing for example „50“ in the PC -> sending data to the controller
3. Using this Information for some operations.
I have a Nucleo-H753ZI Board.
On how to configure my board for this process i found the followed link. Is this the right way for me?
Hope someone could help me.
Kind regards
Arian
2022-12-06 7:01 AM
Hi,
There's some applications on STM32H7 that you can refer to it as an entry point than personalize it according to your need :
TCP Client/Serveur sur NUCLEO-H723ZG
UDP Client/Serveur sur STM32H735G-DK
Regards
Mahdy
2023-01-16 4:57 AM
Greetings !
@AK.10 I am having the exact requirement as yours . If you have already achieved , can you provide suggestions to achieve this .
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.