2022-06-29 2:11 AM
Hello
I am currently developing a card where I need to write logs to an SD card, for this I use an STM32F411 + plus a home made card. First I followed the following tutorial to write on the card:
https://controllerstech.com/interface-sd-card-with-sdio-in-stm32/
this works, but when I wanted to adapt it to use it with RTOS, I always fall in the hardFault_Handler as soon as I get to the f_stat command.
code task:
#include "fatfs.h"
#include "sdio.h"
extern char SDPath[4];
extern FATFS SDFatFS;
extern FIL SDFile;
void task_sd(void *pvParameters){
printf(" ------------------ \r\n");
printf("test carte SD \r\n\r\n");
if (SD_Mount(sd) == HAL_OK){
printf("montage reussi \r\n");
}
SD_CreateFile(sd, "test.txt");
Unmount_SD(sd);
while (1)
{
vTaskDelay(1000);
}
vTaskDelete(NULL);
}function of the library:
HAL_StatusTypeDef SD_CreateFile(char *name){
FIL fil;
FRESULT fresult = f_stat(name, &fno);
if (fresult == FR_OK){ // file already exists
return HAL_ERROR;
}else { // the file does not exist
fresult = f_open(&fil, name, FA_CREATE_ALWAYS|FA_READ|FA_WRITE);
if (fresult != FR_OK){ // file not created
return HAL_ERROR;
}
fresult = f_close(&fil);
if (fresult != FR_OK){ // file not created
return HAL_ERROR;
}
}
return HAL_OK;
}Someone has an idea to help me?
Thank you in advance for your answer
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.