2019-08-31 1:49 AM
This question was asked but it is now closed , so i want to ask again
If some one can share code of how to do sdadc3 for multichannel via
preferred DMA
All code example shows how to work with single channel.
The reason i am asking is that because i tried with DMA and i cannot find any configuration
that DMA start will accept.
it looks to me that SDADC in F373 works only with one channel.
i need the row values from the ADC.
Thanks!
2019-11-12 9:02 PM
I also need this part of the sample program, but there is no answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.