STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

question regarding usb i/o supply in stm32f779ni

Hello,Please consider the following scenario.Let’s say we need different voltage for USB i/o’s. So VDD_USB pin is supplied with separate Vdd_usb supply.Now irrespective of which alternate function in use, does the i/o’s operate in Vdd_usb voltage or ...

STM32Cube USB host library

Hello: I am currently develop on stm32f4/f7 series use USB Host to connect with usb cameras. I found in the STM32Cube USB host library application examples, they all use the USB host with USB DMA disable, then I turn on the USB DMA option in my ...

che.8 by Associate
  • 1158 Views
  • 1 replies
  • 0 kudos

Bug free version of the usb virtual com port driver?

I use the usb device driver for Virtual Com Port v1.0_Cube from STMicroelectronics but the transmission of data with the exact length of 64 bytes (SIZE_SEND_PACKAGE) does not work. Where can I find a bug free version of the driver or a discription of...

BBurg by Associate
  • 1384 Views
  • 2 replies
  • 0 kudos

STM32F103C8Tx / USART1 remap issue

STM32CubeMX : Version 5.3.0Package : STM32CubeF1 Firmware Package V1.8.0Project Settings : Toolchain / IDE = TrueSTUDIO MCU : STM32F103C8TxUSART1 > Mode = Single Wire (Half-Duplex) > Pin usage PB6Lib : LL​In USART1 GPIO Configuration section of USART...

Sam6600 by Associate
  • 992 Views
  • 0 replies
  • 0 kudos

firmware version information

Hello,I am using NUCLEO-F429ZI. I would like to add my application name, author, firmware version and so on information into application profile, how can I add them when I compile the program and save these information into controller? thank you.

yang hong by Associate III
  • 773 Views
  • 1 replies
  • 0 kudos

Resolved! Ethernet controller clock

Sorry for a noob question...The DS for STM32H7 (DS12117 Rev 7, 3.42) says that a PHY can be clocked using 25 MHz from the microcontroller. The PHY we want to use, KSZ8873, has its own connection for 25/50 MHz oscillator. We'd prefer to put only one ...

Pavel A. by Super User
  • 2291 Views
  • 5 replies
  • 0 kudos

HAL legal notices

Hello,I do not know if this question was asked here before so i will apologize in advance for spamming.I want to build an application which is based on the HAL libraries and i do not know if i can use this libraries for free or there is some legal n...

DCipr by Associate
  • 908 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.