2024-02-22 7:44 AM
Hi,
Does any one how to make pbuf’s be in a certain memory range?
For example when I call pbuf_alloc(PBUF_RAW, PBUF_POOL_BUFSIZE, PBUF_POOL) it will allocate a pbuf from a pool that is contained in this array memp_memory, is there a better way/proper way to do this no how I did.
memp.c:
....
/** This is the actual memory used by the pools (all pools in one big block). */
static u8_t memp_memory[MEM_ALIGNMENT - 1
#define LWIP_MEMPOOL(name,num,size,desc) + ( (num) * (MEMP_SIZE + MEMP_ALIGN_SIZE(size) ) )
#include "lwip/memp_std.h"
] __attribute__((section(".my_mem")));
....
I just added __attribute__((section(".my_mem"))), in my linker scrip I have that section tied to an absolute address.
And I'm using lwIP 1.4.0.
Best regards,
Alex
2024-03-06 2:58 AM
Hello @abeslic ,
if you are using CubeIDE the way to set you memory pool in a dedicated memory region has no apparent flows from my side .
but if you want to place the Pbufs in a spesific place in RAM for example you can do the following :
To relocate a pool, declare it as extern in cc.h. Example for GCC:
* extern u8_t \_\_attribute\_\_((section(".onchip_mem"))) memp_memory_my_private_pool_base[];
__attribute__((section(".Rx_PoolSection"))) extern u8_t memp_memory_RX_POOL_base[];
BR
2024-03-06 3:08 AM
With LWIP 2.x and a STM32H733 I'm using this in lwip/arch.h :
in lwip/arch.h:
#ifndef LWIP_DECLARE_MEMORY_ALIGNED
#define LWIP_DECLARE_MEMORY_ALIGNED(variable_name, size) u8_t variable_name[LWIP_MEM_ALIGN_BUFFER(size)] __ATT_SECT_LWIPPOOL
#endif
in main.h:
#define __ATT_SECT_LWIPPOOL __attribute__((section(".LwipPoolSection")))
in linker file:
SRAXI_D1(xrw) : ORIGIN = 0x24000000, LENGTH = 320K
...
/* lwIP POOL section */
.LwipPoolSection (NOLOAD):
{
. = ALIGN(4);
*(.LwipPoolSection)
*(.LwipPoolSection*)
. = ALIGN(4);
} >SRAXI_D1
/* } >SRAXI_D1_LWIP */
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.