2026-03-23 10:41 AM - last edited on 2026-03-27 6:24 AM by mƎALLEm
Hi Everyone,
I one of our project i want to store the logs on NOR flash. I want to use Levelx to take care of NOR flash low level . But as per documents levelx can be used with Filesx, Is there is any way that i can use Levelx with Filex?
2026-03-23 11:21 AM - edited 2026-03-23 11:26 AM
@Harwinder2312 wrote:Is there is any way that i can use Levelx with Filex?
You mean without ?
So it looks like you'll have to work direct from the Eclipse documentation to do that ...
2026-03-24 3:30 AM
Yes on St wiki it says it must use with filex, that's why i asked. Thank you for other references. I will try and update you one this. Thanks
2026-03-24 3:40 AM
@Harwinder2312 wrote:Yes on St wiki it says it must use with filex
Probably what they mean is, that's the only way ST provide support via CubeMX - if you want it standalone, then you have to do that manually, on your own.
Like this.
2026-03-24 3:42 AM
Yes you are right, this point is also in my mind, I will try both ways and update you which one works for me. Thanks
2026-03-27 6:22 AM
Hi @Harwinder2312,
Could you please provide more details on how you plan to use LevelX alone?
Please keep in mind that LevelX doesn't have any filesystem logic.
regards
Haithem.
2026-03-27 6:33 AM
Hi Haithem,
Let me explain bit details. I am working on an HVAC system where i need to store all logs of HVAC system with time stamp. Earlier i was using EEprom, as you know in eeprom has size problem. This time i want to use OSPi Flash, as i am working with STM32H573 MCU. I have seen the DK board for same series and using same OSPi with 512Mb size. We have provision of USB drive to download logs. For USb drive i am using filex to MSC class to save CSV file in USB drive. On flash side i want to use Levelx only to protect sectors,. as its mentioned in documents of Levelx that it take care of flash with rotation of sectors also power failure snario . So that is the main purpose of using levelx. If you have some better idea please suggest i am happy to listen you view point on this. Any advice will be helpful. I you need more information i am happy to share as well.
Thanks
2026-03-27 7:09 AM
So, if you already have FileX, why not use it for storing your logs?
2026-03-27 8:49 AM
There are two reasons, one is this is my first time i am using filex so i don't know much how to use it for two instances(one for Flash and other for USB). Second may be i am wrong i don't want to overload flash by file system.
2026-03-27 9:43 AM - edited 2026-03-27 9:44 AM
Hi
thanks indeed for this fruitful discussion, really appreciate it.
- Here is the link to an application on STM32H573-DK running 2 FileX instances. (uSD + OSPI).
@Harwinder2312 wrote:On flash side i want to use Levelx only to protect sectors,. as its mentioned in documents of Levelx that it take care of flash with rotation of sectors also power failure snario.
@Harwinder2312 wrote:There are two reasons, one is this is my first time i am using filex so i don't know much how to use it for two instances(one for Flash and other for USB). Second may be i am wrong i don't want to overload flash by file system.
If I understand correctly, you want to use LevelX to write log data into LevelX logical sectors to benefit from LevelX wear leveling without the overhead of a file system. If that is the case, I'm afraid this won't work, as doing so will make access to the log data quite difficult since the logs will be spread throughout the entire OCTOSPI. The mapping between LevelX logical sectors and physical addresses is managed internally by LevelX.
Thus you'll need a filesystem on the NOR Flash too to keep your logs structured accessible easily by the application.
Hope this helps
Haithem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.