2025-05-13 11:38 PM - last edited on 2025-05-30 3:02 AM by Amel NASRI
Hi Mike,
Thanks again for your previous support on the SPI interface.
I have since moved to using the SDMMC interface instead of SPI for better performance, but I am still facing issues.
Current Issue Summary:
I can successfully mount the 32GB SDHC FAT32 card and read the capacity using FatFs.
However, f_write always fails.
After debugging, I found that BSP_SD_WriteBlocks fails when writing to LBA 32768.
I also verified this with direct HAL_SD_WriteBlocks, which fails at LBA 32768 but works on lower LBAs like 0 or 1.
This suggests the problem is not in FatFs logic, but rather in high LBA (large address) block access stability.
My Questions:
Is this a known limitation with STM32H7 SDMMC or HAL drivers when writing to higher LBA regions on large-capacity SD cards (like 32GB)?
Looking forward to your insights.
Best regards,
Han
Edit: Moved from STM32H753ZI SPI SD Card Not Responding to CMD0/CMD8 (0xFF Response)
Solved! Go to Solution.
2025-05-28 7:14 AM - edited 2025-05-28 7:14 AM
Hello @HANITALY
Did you try to communicate with the SD card only with HAL SDMMC before using FatFs?
2025-05-28 7:14 AM - edited 2025-05-28 7:14 AM
Hello @HANITALY
Did you try to communicate with the SD card only with HAL SDMMC before using FatFs?
2025-05-28 8:14 AM
Hi, I actually have solved the issue, forgot to deleted this post.
Thank you for the reply!
2025-05-30 3:03 AM
Hi @HANITALY ,
Glad to know that the faced issue is already fixed.
It would be interesting if you can share the solution with our community.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-13 9:03 AM
Hi,
It has been a while, I only recall that I set SDMMC_BUS_WIDE from 4B to 1B, and connected physically only the D0 pin to the board, then it worked.
static void MX_SDMMC1_SD_Init(void)
{
/* USER CODE BEGIN SDMMC1_Init 0 */
/* USER CODE END SDMMC1_Init 0 */
/* USER CODE BEGIN SDMMC1_Init 1 */
/* USER CODE END SDMMC1_Init 1 */
hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 32;
/* USER CODE BEGIN SDMMC1_Init 2 */
/* USER CODE END SDMMC1_Init 2 */
}
This is the configuration that worked.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.