2025-04-08 9:21 PM
Hi everyone, I am using STM32H745BIT6 and programming using W25Q128. I am trying to upload the code but always get an error at the last step.
STMicroelectronics ST-LINK GDB server. Version 7.10.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number: 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
Log output file: C:\Users\hieua\AppData\Local\Temp\STM32CubeProgrammer_a22168.log
ST-Link Server is running on port : 7184
ST-LINK SN : 130019000D0000383036544E
ST-LINK FW : V2J46S7
Board : --
Voltage : 3.10V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name: STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x91
Opening and parsing file: ST-LINK_GDB_server_a22168.srec
Memory Programming...
File : ST-LINK_GDB_server_a22168.srec
Size : 4.98 KB
Address : 0x08100000
Erasing memory corresponding to sector 0:
Erasing internal memory sector 8
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:03.382
Verifying...
Download verified successfully
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
Log output file: C:\Users\hieua\AppData\Local\Temp\STM32CubeProgrammer_a22168.log
ST-Link Server is running on port : 7184
ST-LINK SN : 130019000D0000383036544E
ST-LINK FW : V2J46S7
Board : --
Voltage : 3.10V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name: STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x91
Opening and parsing file: ST-LINK_GDB_server_a22168.srec
Memory Programming...
File : ST-LINK_GDB_server_a22168.srec
Size : 185.59 KB
Address : 0x08000000
Erasing memory corresponding to sector 0:
Erasing internal memory sectors [0 1]
Erasing memory corresponding to sector 0:
Erasing external memory sector 0
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening E:\STM32\IDE\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.100.202412061334\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
I have referenced the build here: https://controllerstech.com/w25q-flash-series-part-10-qspi-ext-loader-in-h750/ and https://www.youtube.com/watch?v=XqCq0xtQmbI&list=PLnMKNibPkDnHIrq5BICcFhLsmJFI_ytvE&index=7
2025-04-08 9:38 PM
@NguyenAnhHieu_ You selected wrong stldr file. try to get correct external loader from https://github.com/cturvey/stm32extldr/blob/main GIT.
2025-04-08 9:50 PM
Thanks, but unfortunately when designing the hardware I chose a pin configuration that was completely different from the pre-made files. So I had to find a way to create the .stldr file
2025-04-18 3:24 AM
Hello @NguyenAnhHieu_ ;
->So I had to find a way to create the .stldr file
I recommend you to look at How to create an external QSPI loader MOOC and get inspired to create the own .stldr file. This MOOC explains how to create an external QSPI loader for STM32CubeProgrammer.
I hope this help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.