2019-08-06 11:27 PM
I have the following couple of questions
QUESTION :1) what is the difference between USB drivers in the cubemx standard hal library middleware and CMSIS USB Middleware based on the following 2 cases?
CASE:1) In STM32CUBEMX, When I use STM32 standard Hal library for USB device (through generate code option) , I get USB driver enumerated properly. Send and receive characters works fine with USB serial device com port terminal.
CASE:2) But If I use CMSIS Middleware USB Device and CMSIS FreeRTOS, the enumeration is happening with Inverted or unresolved yellow symbol as shown in attached pictures in USB Serial Device(COM7) in device manager(Other than thread API code is same as USB Device Virtual Com Port example code provided by arm keil). Does CMSIS Middleware USB device requires any host drivers?
QUESTION:2) I checked in the USB Device Virtual Com Port example code provided by arm keil which uses CMSIS USB Middleware abd CMSIS RTOS from the link http://www.keil.com/pack/doc/mw/USB/html/dev_cdc_tutorial.html and in their example source folder, I could find the following 3 files.
I would like to know why there is a need for INF file(VID & PID info) in this CMSIS Middleware and why these are not needed for stm32cubemx GUI based USB hal drivers.
Iam stuck in this for more than a weeks time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.