2023-04-04 9:35 PM
2023-04-04 9:40 PM
Push in via an External Loader, pull via Ethernet, or USB Flash Drive (MSC Host)
2023-04-04 11:07 PM
Do you have a sample?
2023-04-05 2:00 AM
Not something I'm working on. Perhaps look if there is an example MSC Device using the eMMC directly?
2023-04-06 7:27 AM
Hello @wsuwa.1,
For audio file, you can get inspired with the example provided for STM32H747I-DISCO as referenced here.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.