2025-04-24 8:40 AM - last edited on 2025-04-24 8:58 AM by TDK
I AM TRYING TO CONTROL WITH CLRC SPI. MY PROJECT IS WRITTEN WITH LL. I CANNOT ADAPTE THIS FUNCTION. CAN YOU PLEASE HELP ME?
2025-04-29 6:53 AM
These are the codes I tried to use to replace HAL_SPI_TransmitReceive with LL-based code, but they are not working. How can I explain this more clearly? I can receive data from my CLRC663 module using full-duplex communication with HAL, but I cannot receive anything with the LL version.
uint8_t SPI2_ByteSend (uint8_t val)
{
LL_SPI_TransmitData8(SPI2, val);
while (LL_SPI_IsActiveFlag_BSY(SPI2));
return(LL_SPI_ReceiveData8(SPI2));
}
void mfrc630_SPI_transfer(const uint8_t* tx, uint8_t* rx, uint16_t len)
{
LL_GPIO_ResetOutputPin(SPI2_NSS_GPIO_Port, SPI2_NSS_Pin); // Slave Select aktif
for (uint16_t i = 0; i < len; i++) {
if (rx != NULL) {
rx[i] = SPI2_ByteSend(tx[i]);
} else {
(void)SPI2_ByteSend(tx[i]); // RX kullanilmiyorsa sadece gönder
}
}
LL_GPIO_SetOutputPin(SPI2_NSS_GPIO_Port, SPI2_NSS_Pin); // Slave Select deaktif
}
I WANT TO RUN THIS LIBRARY:https://github.com/CodElecCz/STM32F1-CLRC663
2025-04-29 6:58 AM
I found an example related to STM32L4, and I think the issue is related to DMA. After the first bit is sent, the slave responds immediately, but the processor misses it. This needs to be handled with DMA to avoid the issue. However, I couldn't find a suitable LL-based example. I need to rewrite the HAL_SPI_TransmitReceive function using LL, whether with DMA or another method—but it must do exactly the same job without missing anything.
HAL_SPI_TransmitReceive(&hspi2, tx, rx, len, 1000)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.