2024-04-15 3:29 AM
How should a new STM32H747I-DISCO be used, why does the display not start after I connect the computer with st-link and display 32kb of memory
2024-05-22 9:36 AM
Hello @beijing,
To prevent ST-Link connection problems, confirm that your development environment is configured for the appropriate target device. Additionally, regularly update the embedded firmware to access new features or corrections. Detailed information is available in the ST-LINK derivatives technical note (TN1235) on st.com.
For proper booting, verify the boot jumpers on the board are set correctly to boot from the designated memory. For detailed guidance on configuring and resolving issues with the display, refer to the STM32H747I-DISCO user manual (UM2411) on st.com.
Thanks and Best Regards,
Dorsaf
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.