STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NMI HANDLER

Hiwith STM32H563ZI, (nucleo-h563) I work on freertos + tcp, when I try to make flash operation like erasing software goes NMI handler, but if not making erase just make flash_program it doesnt fail, because of I couldnt erase the sectorsi I cant prog...

Recep by Associate II
  • 1316 Views
  • 0 replies
  • 0 kudos

Programming a STM32 F405 flight controller - Mateksys F405-Te - Can't upload code from STM32CubeIDE

Hello :)For my university project, I need to build a drone. I've never done anything like this before and could use a bit of a jumpstart.I have a Mateksys F405-TE flight controller that I'm supposed to use to control the drone.To test it, I created a...

write to flash fail

Hi,I try to write and read from flash on stm32wb10cc but when i try to write by HAL_FLASH_Program function i received 3 errors in  FLASH Status register:1. Programming alignment error2. size error3. Programming sequence error my code is: on the main:...

aviel by Associate II
  • 1845 Views
  • 1 replies
  • 0 kudos

Resolved! TCP Client

Hello I'm developing a TCP client for STM32F4 MCU.I'm using the LWIP sockets api and freeRTOS to do so.This client will both send and receive data when triggered by RTC (every hour or so) and based on an ADC reading.My understanding is both sockets a...

USB CDC BAREMETAL

Hello everyone, Here i'm trying to implement USB CDC FS on STM32F107VCT6 using Standard Library(without HAL Library), but when i am trying to initialize clock for USB (RCC_APB1ENR_USBEN) its showing error that this register is not available for Conne...

Pkush.1 by Associate
  • 2057 Views
  • 2 replies
  • 0 kudos

Resolved! Interrupt Service Routine Jitter

Hi,I use a STM32F767 Nucleo-144 board with a STM32F767ZIT6 processor.With CubeIDE I configure SPI1 as I2S1 input and pump the data via DMA2/Stream0  in a short 8x16Bit circular buffer. The clock of the SPI1 is at ~ 3MHz .I set up the HAL_I2S_RxHalfCp...

DetlefS by Senior
  • 9610 Views
  • 22 replies
  • 2 kudos

Resolved! Microsecond delay for STM32G030F6P6TR

Hello I am trying to work with Microseconds delay in my codeso follow this very help full post on web POSTand I configure TIMER 3 ( I have also check with all available timer )But unfortunately, it doesn't work for my STM32GO3O MCU /* USER CODE BEGIN...

sandeep3 by Associate II
  • 6980 Views
  • 5 replies
  • 2 kudos

STM32L072 Standby Mode problems

Hello!I'm using the DISCO-L072CZ-LRWAN1 board and have some trouble using the low power modes.It seems whenever i enter the low power mode, it immediately wakes up again, I've tried following a few of the guides and can't see what I'm doing wrong. Th...

Fiskk by Associate
  • 2500 Views
  • 3 replies
  • 0 kudos

ETH HTTP CLIENT

Hello, I have created a project about eth http as a server as well. stm32h750b-dkI have created a web page. Then I wanted to develop the ability to connect to the phpmyadmin database. I tried writing code with html and javascript (the reason I used j...

non by Associate III
  • 1300 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.