2023-05-01 6:14 AM
Hi
I have upgraded my STMCUBE to the latest version of 6.8.1 and am Using STM32H750XBH6 part, when I try to config the CPU clock to 480Mhz, it raises many error flags and would not allow it (also the Resolve clock Issues Button can not fix it), Note my Device is version Y and I could do it easily in 6.6.1 version.
I want to use the stm32cube_fw_h7_v1110 package, so I need to upgrade the CUBE, is there any work around this?
2023-05-01 7:27 AM - edited 2023-11-20 6:45 AM
depending on version they set a (new) limit;
+ you set..scale0 ?
2023-05-01 7:40 AM
I thought Y was rated at 400 MHz, and V was 480 MHz
>>is there any work around this?
You could ignore it, and fix the generated code to the speeds you want
2023-05-01 7:47 AM
AScha.a When I choose the PPL the power regulator setting would go away,
Thanks Tesla DeLorean, How Can I do it?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.