2020-06-08 1:00 PM
Hi,
I have an application where general-purpose DMA (triggered by TIM peripheral) timing is critical. I found that when there's communication over Ethernet, the timing requirements for the GP DMA are occasionally not met. I'm thinking that this might be an arbitration/priority issue between the Ethernet DMA and the GP DMA. Is this possible? Can an Ethernet DMA transfer block GP DMA transfers? If yes, how do I give priority to the GP DMA over the Ethernet DMA? I'd appreciate any pointers.
Thanks, Szabi
2020-06-08 1:53 PM
Which 'F4?
> Can an Ethernet DMA transfer block GP DMA transfers?
Yes, to certain extent, if it uses bursts. See ETH_DMABMR and Host bus burst access subchapter of ETH chapter in RM.
Other than that, it's one of the masters on the busmatrix, which is said to be round-robin arbitrated, so if ETH and CPU and the second DMA attempts to access the same memory in the same moment than your "critical" DMA, it will be delayed by 3 AHB cycles (assuming you have no LTDC and HS_USB with enabled DMA).
A simple way to avoid collision with ETH is to use a different SRAM. You have at least two probably in every 'F4 which has ETH.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.