2019-01-10 8:31 AM
Hi,
i generated HAL code with the latest version of stm32cubemx and the latest stm32f4 software package.
In the pinout configuration of stm32cubemx i checked the temperature channel, therefore the vbat is unchecked.
Using the function HAL_ADC_ConfigChannel of stm32f4xx_hal_adc.c to set the channels and corresponding ranks to read, i set for example the ADC_CHANNEL_TEMPSENSOR channel.
That channel is defined as channel 18 in stm32f4xx_hal_adc_ex.h:
#if defined(STM32F413xx) || defined(STM32F423xx)
#define ADC_CHANNEL_TEMPSENSOR ((uint32_t)ADC_CHANNEL_18)
#endif /* STM32F413xx || STM32F423xx */ ,
which corresponds to the reference manual.
The vbat channel is as well channel 18 due to reference manual and set in stm32f4xx_hal_adc.h:
#define ADC_CHANNEL_VBAT ((uint32_t)ADC_CHANNEL_18)
If the vbate bit is now set in the CCR register of the ADC, channel18 outputs the vbat value instead of temperature.
In the function HAL_ADC_ConfigChannel now on input ADC_CHANNEL_TEMPSENSOR of the sConfig the software does not distinguish between ADC_CHANNEL_TEMPSENSOR and ADC_CHANNEL_VBAT as both are defined as ADC_CHANNEL_18. The vbate bit is therefore set and temperature not read, instead the vbat value:
HAL_StatusTypeDef HAL_ADC_ConfigChannel(ADC_HandleTypeDef* hadc, ADC_ChannelConfTypeDef* sConfig)
{
__IO uint32_t counter = 0U;
ADC_Common_TypeDef *tmpADC_Common;
/* Check the parameters */
assert_param(IS_ADC_CHANNEL(sConfig->Channel));
assert_param(IS_ADC_REGULAR_RANK(sConfig->Rank));
assert_param(IS_ADC_SAMPLE_TIME(sConfig->SamplingTime));
/* Process locked */
__HAL_LOCK(hadc);
/* if ADC_Channel_10 ... ADC_Channel_18 is selected */
if (sConfig->Channel > ADC_CHANNEL_9)
{
/* Clear the old sample time */
hadc->Instance->SMPR1 &= ~ADC_SMPR1(ADC_SMPR1_SMP10, sConfig->Channel);
/* Set the new sample time */
hadc->Instance->SMPR1 |= ADC_SMPR1(sConfig->SamplingTime, sConfig->Channel);
}
else /* ADC_Channel include in ADC_Channel_[0..9] */
{
/* Clear the old sample time */
hadc->Instance->SMPR2 &= ~ADC_SMPR2(ADC_SMPR2_SMP0, sConfig->Channel);
/* Set the new sample time */
hadc->Instance->SMPR2 |= ADC_SMPR2(sConfig->SamplingTime, sConfig->Channel);
}
/* For Rank 1 to 6 */
if (sConfig->Rank < 7U)
{
/* Clear the old SQx bits for the selected rank */
hadc->Instance->SQR3 &= ~ADC_SQR3_RK(ADC_SQR3_SQ1, sConfig->Rank);
/* Set the SQx bits for the selected rank */
hadc->Instance->SQR3 |= ADC_SQR3_RK(sConfig->Channel, sConfig->Rank);
}
/* For Rank 7 to 12 */
else if (sConfig->Rank < 13U)
{
/* Clear the old SQx bits for the selected rank */
hadc->Instance->SQR2 &= ~ADC_SQR2_RK(ADC_SQR2_SQ7, sConfig->Rank);
/* Set the SQx bits for the selected rank */
hadc->Instance->SQR2 |= ADC_SQR2_RK(sConfig->Channel, sConfig->Rank);
}
/* For Rank 13 to 16 */
else
{
/* Clear the old SQx bits for the selected rank */
hadc->Instance->SQR1 &= ~ADC_SQR1_RK(ADC_SQR1_SQ13, sConfig->Rank);
/* Set the SQx bits for the selected rank */
hadc->Instance->SQR1 |= ADC_SQR1_RK(sConfig->Channel, sConfig->Rank);
}
/* Pointer to the common control register to which is belonging hadc */
/* (Depending on STM32F4 product, there may be up to 3 ADCs and 1 common */
/* control register) */
tmpADC_Common = ADC_COMMON_REGISTER(hadc);
/* if ADC1 Channel_18 is selected enable VBAT Channel */
if ((hadc->Instance == ADC1) && (sConfig->Channel == ADC_CHANNEL_VBAT))
{
/* Enable the VBAT channel*/
tmpADC_Common->CCR |= ADC_CCR_VBATE;
}
/* if ADC1 Channel_16 or Channel_17 is selected enable TSVREFE Channel(Temperature sensor and VREFINT) */
if ((hadc->Instance == ADC1) && ((sConfig->Channel == ADC_CHANNEL_TEMPSENSOR) || (sConfig->Channel == ADC_CHANNEL_VREFINT)))
{
/* Enable the TSVREFE channel*/
tmpADC_Common->CCR |= ADC_CCR_TSVREFE;
if((sConfig->Channel == ADC_CHANNEL_TEMPSENSOR))
{
/* Delay for temperature sensor stabilization time */
/* Compute number of CPU cycles to wait for */
counter = (ADC_TEMPSENSOR_DELAY_US * (SystemCoreClock / 1000000U));
while(counter != 0U)
{
counter--;
}
}
}
/* Process unlocked */
__HAL_UNLOCK(hadc);
/* Return function status */
return HAL_OK;
}
What am i missing? Is there any additional configuration i have to make somewhere?
Regards, Kjell Pirschel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.