STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I want to know regarding external clock stabilization time/Delay, I am facing USB comport detection issue in STM32F070RBMCU.

Issue with the customized board is that, it does not detects USB(FS CDC) comport every time as we plug/unplug the device.whereas the same firmware works fine with ST nucleo board of STM32F070RBTx.1. Do programmer needs to add any additional delay for...

GDube by Associate
  • 858 Views
  • 0 replies
  • 0 kudos

Problem with upload program via usb dfu

Hi guys,I have a problem with updating stm32f407vg disco board via usb dfu, I generate the project from cubemx and I'm looking at the example from ST: en.stm32cubef4\STM32Cube_FW_F4_V1.21.0\Projects\STM324xG_EVAL\Applications\USB_Device\DFU_Standalon...

BWawr by Associate II
  • 612 Views
  • 0 replies
  • 0 kudos

How to use FLASH_OB_UserConfig() API ?

Hi, It may sound like a minor query to many of you, but can any one explain me what are 'UserType' and 'UserConfig' parameters in FLASH_OB_UserConfig() API ?Some how I can't get their meanings.I am working on STM32L432KB and want my system to boot fr...

Bootloader does not work after power cycle

I am trying to use the built in bootloader on an STM32H750VB over USART1. I've used the code found here to enter the bootloader,https://community.st.com/s/question/0D50X00009XkW8QSAV/stm32h743-how-to-start-the-system-boot-loader-via-softwareI've been...

ELars by Associate
  • 3273 Views
  • 5 replies
  • 0 kudos

NUCLEO-L476RG as USB FS serial device

Is the CN1 USB Mini-B connector on the NUCLEO-L476RG board also connected to the STM32L476 target? Or it is only for ST-LINK-V2-1 section.If the CN1 connector is only for ST-LINK-V2-1 then one has to solder a USB socket to the STM32L476 target to use...

MSuhe by Associate III
  • 1610 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.