2021-08-30 1:59 PM
I am trying to use Sockets under FreeRTOS. Currently can send data over UDP using netconn, but sockets only send information when two netconn messages are sent previous to the socket one. If some of the netconn_sendto(...) functions is commented, sendto stops working.
void UDP_Send_Thread(void)
{
// Creamos estructuras de datos necesarias para los envíos
struct netconn *conn;
struct netbuf *outbuf;
u8_t dataraw[] = "Hola UDP RTOS\n";
// Generamos IP para envío de datos
ip_addr_t ipto;
IP4_ADDR(&ipto,172,16,0,2);
// Creamos conexión UDP con netconn
conn = netconn_new(NETCONN_UDP);
int s = socket(AF_INET, SOCK_DGRAM, 0);
struct sockaddr_in addr, cliaddr;
memset(&addr, 0, sizeof(addr));
memset(&cliaddr, 0, sizeof(cliaddr));
addr.sin_family = AF_INET;
addr.sin_addr.s_addr = IP_ADDR_ANY;
addr.sin_port = htons(60000);
cliaddr.sin_family = AF_INET;
cliaddr.sin_addr.s_addr = inet_addr("172.16.0.2");
cliaddr.sin_port = htons(49002);
int b = bind(s, (const struct sockaddr *) &addr, sizeof(addr));
// Creamos buffer para envío de datos de tipo netbuf
outbuf = netbuf_new();
// referenciamos cadena de texto al buffer
netbuf_ref(outbuf, dataraw, sizeof(dataraw));
for(;;)
{
// Enviamos datos
netconn_sendto(conn, outbuf, &ipto, 49000);
netconn_sendto(conn, outbuf, &ipto, 49001);
osDelay(500);
// Indicamos con un LED que el envío se ha hecho (parpadeo)
sendto(s, dataraw, strlen(dataraw), MSG_DONTWAIT, (const struct sockaddr *) &cliaddr, sizeof(cliaddr));
HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
osDelay(500);
}
}Can somebody help me regarding with this issue? I am trying to learn how to use all Raw, Sockets and Netconn LWIP.
Thanks in advance.
2021-09-03 9:25 AM
I solved the issue... Following code works fine sending standalone Sockets messages and Messages in conjunction with netconn
int Eth_UDP_Init(int port)
{
int on = 1; // On value for SO_BROADCAST
struct sockaddr_in sockin;
int sd = socket(AF_INET, SOCK_DGRAM, 0); // Init a Socket descriptor
memset((uint8_t *) &sockin, 0, sizeof(sockin)); // Reset all sockin values to zero
sockin.sin_family = AF_INET;
sockin.sin_port = htons(port); // htons() converts int to host port information
/* Bind a name to the socket */
if( bind(sd, (struct sockaddr*) &sockin, sizeof(sockin)) == -1 )
{
printf("Error on socket binding: %d \n", port);
return 0;
}
printf("Socket binded for port %d \n", port);
/* Socket options:
* - SOL_SOCKET: To manipulate options at "Socket" level
* - SO_BROADCAST: To send data to more than one destination */
setsockopt(sd, SOL_SOCKET, SO_BROADCAST, &on, sizeof(on));
return sd; // returns socket descriptor
}
long UDP_Send(int sd, char *buf, int buflen, char *ipdest, int portdest)
{
struct sockaddr_in servaddr; // Destination descriptor
servaddr.sin_family = AF_INET;
servaddr.sin_port = htons(portdest);
servaddr.sin_addr.s_addr = inet_addr(ipdest);
return sendto(sd, buf, buflen, 0, (struct sockaddr*) &servaddr, sizeof(servaddr) ); // send to an specific source
}
void UDP_Send_Thread(void)
{
// Creamos estructuras de datos necesarias para los envíos
struct netconn *conn;
struct netbuf *outbuf;
int sd, sd2;
u8_t dataraw[] = "Hola UDP RTOS\n";
// Generamos IP para envío de datos
ip_addr_t ipto;
IP4_ADDR(&ipto,172,16,0,2);
// Creamos conexión UDP con netconn
conn = netconn_new(NETCONN_UDP);
sd = Eth_UDP_Init(60000);
sd2 = Eth_UDP_Init(50000);
// Creamos buffer para envío de datos de tipo netbuf
outbuf = netbuf_new();
// referenciamos cadena de texto al buffer
netbuf_ref(outbuf, dataraw, sizeof(dataraw));
for(;;)
{
// Enviamos datos
netconn_sendto(conn, outbuf, &ipto, 49000);
netconn_sendto(conn, outbuf, &ipto, 49001);
UDP_Send(sd, dataraw, strlen(dataraw), "172.16.0.2", 60001);
UDP_Send(sd2, "Hola SD2", strlen("Hola SD2"), "172.16.0.2", 60001);
osDelay(500);
// Indicamos con un LED que el envío se ha hecho (parpadeo)
HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
osDelay(500);
}
}Hope can help you to face issues like mine
:)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.