2021-08-05 12:10 AM
Hi ,
I want configure the UART and GPIO peripherals using RTOS(RTx) .
here I am using keil5 u version .And STM32F217xx controller (custom board )
Already I was done configuration for gpio.
/*----------------------------------------------------------------------------
* CMSIS-RTOS 'main' function template
*---------------------------------------------------------------------------*/
#include "RTE_Components.h"
#include CMSIS_device_header
#include "cmsis_os2.h"
void gpio_Initfun(void);
/*
* led initialization.
*
*/
void gpio_Initfun(void)
{
GPIOF->MODER |=0x00000005;
GPIOF->OTYPER |=0x00000000;
GPIOF->OSPEEDR |=0x00000005;
GPIOF->PUPDR |=0x00000005;
GPIOF->ODR |=0x000000000;
}
/*----------------------------------------------------------------------------
* Application functions thread
*---------------------------------------------------------------------------*/
__NO_RETURN static void ledTwo (void *argument) {
(void)argument;
while(1)
{
osDelay(500);
GPIOF->ODR &= ~(unsigned int)(0x0000001);
osDelay(500);
GPIOF->ODR |= 0x0000001;
}
}
__NO_RETURN static void ledOne (void *argument) {
(void)argument;
while(1)
{
osDelay(500);
GPIOF->ODR &= ~(unsigned int)(0x0000002);
osDelay(500);
GPIOF->ODR |= 0x0000002;
}
}
int main (void) {
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOFEN);
SystemCoreClockUpdate();
osKernelInitialize();
gpio_Initfun();
osThreadNew(ledTwo, NULL, NULL);
osThreadNew(ledOne, NULL, NULL);
osKernelStart();
while(1);
}the above code is working.
Instead of using the SFR programming I want to use predefined librariesf or programming the my controller.
Please some one guide me how to use STM32 predefined libraries in RTOS programming.
thanks in advance.
Solved! Go to Solution.
2021-08-06 5:20 AM
Hi,
You can refer to provided FreeRTOS examples within STM32CubeF2 firmware via this path: STM32Cube_FW_F2_V1.8.0\Projects\STM322xG_EVAL\Applications\FreeRTOS
Bouraoui
2021-08-06 5:20 AM
Hi,
You can refer to provided FreeRTOS examples within STM32CubeF2 firmware via this path: STM32Cube_FW_F2_V1.8.0\Projects\STM322xG_EVAL\Applications\FreeRTOS
Bouraoui
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.