2025-01-03 2:10 AM
Hello ,
I am working on a project with the STM32L562CET6 microcontroller and have encountered an issue with the timer interrupt callback function.
1. I configured TIM6 as the clock source for the microcontroller. Consequently, the HAL_TIM_PeriodElapsedCallback() function is automatically triggered whenever the TIM6 interrupt occurs.
2. Now, I have configured TIM2 for a different purpose, but I noticed that when the TIM2 interrupt occurs, the same HAL_TIM_PeriodElapsedCallback() is triggered.
Since the HAL_TIM_PeriodElapsedCallback() is defined with the weak attribute, I understand that I can redefine it in my user code. However, this causes conflicts when multiple timers (like TIM6 and TIM2) trigger this callback.
Questions:
1. Is there a way to alias or redirect the HAL_TIM_PeriodElapsedCallback() to separate functions for different timers (e.g., one for TIM6 and another for TIM2)?
2. Is there any other specific callback function available for timers in STM32 HAL that can help separate the interrupt handling for different timers?
3. What is the recommended approach to handle multiple timers efficiently without such conflicts?
Thank you !
Solved! Go to Solution.
2025-01-03 6:34 AM - edited 2025-01-03 6:35 AM
Hello @Sankar_Eswaran
You can configure the register callback to call the user defined callback function.
HAL_TIM_RegisterCallback(&htim2, HAL_TIM_PERIOD_ELAPSED_CB_ID, User_TIM2PeriodElapsedCallback);
HAL_TIM_RegisterCallback(&htim6, HAL_TIM_PERIOD_ELAPSED_CB_ID, User_TIM6PeriodElapsedCallback);
To use this feature, you should set the flag USE_HAL_TIM_REGISTER_CALLBACKS to 1.
2025-01-03 5:47 AM
Hello @Sankar_Eswaran,
Generally, this is how we handle multiple interrupts:
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == TIM2) {
code
}
if (htim->Instance == TIM6) {
code
}
}
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-03 6:34 AM - edited 2025-01-03 6:35 AM
Hello @Sankar_Eswaran
You can configure the register callback to call the user defined callback function.
HAL_TIM_RegisterCallback(&htim2, HAL_TIM_PERIOD_ELAPSED_CB_ID, User_TIM2PeriodElapsedCallback);
HAL_TIM_RegisterCallback(&htim6, HAL_TIM_PERIOD_ELAPSED_CB_ID, User_TIM6PeriodElapsedCallback);
To use this feature, you should set the flag USE_HAL_TIM_REGISTER_CALLBACKS to 1.
2025-01-06 5:12 AM
Thank you...
2026-05-20 2:07 AM
Which way is more efficient? Registering different callbacks for each timers vs. having a singular callback which branches based on the timer responsible for the callback.
2026-05-20 2:56 AM - edited 2026-05-20 2:57 AM
Neither. Cube/HAL is not meant to be efficient, either way; it's meant to be convenient and portable between STM32 models/families.
Individual timers naturally have individual interrupt vectors(*). Cube/HAL's architecture makes them call a single "resolving" function, which then in turn calls either the singular callback where you would branch, or the registered callbacks where the very same branching is performed in that "resolving" function.
So, if you want efficiency, simply avoid Cube/HAL.
JW
(*) with some exceptions, depending on the given STM32 model/family
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.