2021-02-23 8:45 AM
Hi!
I'm using STM32H7 for a new project, and I need to send data through HAL_SPI_Transmit_DMA to an external MRAM.
I have a block of 34000 bytes. If i send this: HAL_SPI_Transmit_DMA(&MRAM_SPI_H, buf, 34000); there is some write problem (when I read the data, some bit is changed so the CRC error takes place).
However, If i send the same block of data but divided in few parts (for example, parts of 5000 bytes): HAL_SPI_Transmit_DMA(&MRAM_SPI_H, buf, 5000) then the data reading is completely correct.
The maximum size of the SPI transaction is uint16_t so, what could be the problem?
Thank you so much in advance
Josep
Solved! Go to Solution.
2021-02-24 3:48 AM
Solved.
The problem was the timeout value of the reading function. The reading is using regular SPI HAL_SPI_Receive and the timeout value wasn't enough for the 34KB.
Thank you
2021-02-23 9:56 AM
>>what could be the problem?
Cache coherency? MPU memory region setting?
Does the memory device have a transactional limit or timeout?
2021-02-24 3:48 AM
Solved.
The problem was the timeout value of the reading function. The reading is using regular SPI HAL_SPI_Receive and the timeout value wasn't enough for the 34KB.
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.