2019-05-01 2:31 AM
Hello everyone!!!
I get a problem with HAL_Delay function. When I use STM32CubeMX creat my simple project (blink a led with STM32F4 Discovery Kit) everything is OK with HAL_Delay() function.
But when I creat a same project without using STM32CubeMX, HAL_Delay() function seem not working. I don't know why.
Anyone can help me!! Thank you very much!!!!
2019-05-01 2:41 AM
Make your own delay using basic timer and dependencies may decrease.
2019-05-01 2:43 AM
Make sure to initialize the SysTick interrupt and that the interrupt calls the HAL functions to advance the internal tick count.
2019-05-01 2:48 AM
I have created project by STM32CubeMX but I can't find SysTick interrupt but it is OK. I copy this code to Keil uVision5 and HAL_Delay() not working.
2019-05-04 3:25 PM
You can put this to main.c, it works for me:
void SysTick_Handler(void) {
HAL_IncTick();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.