2019-05-05 12:40 AM
I'm working on a project using a STM32F446 with a boilerplate created with STM32CubeMX (for peripherals initialization and middleware like the FreeRTOS with the CMSIS-V1 interface). I have two threads which communicate using mailboxes but I encountered a problem: one of the thread body is (I made it more understandable)
void StartDispatcherTask(void const * argument)
{
mailCommand *commandData = NULL;
mailCommandResponse *commandResponse = NULL;
osEvent event;
for(;;)
{
event = osMailGet(commandMailHandle, osWaitForever);
commandData = (mailCommand *)event.value.p;
// Here is the problem
osDelay(5000);
}
}It gets to the delay but never gets out. Is there a problem with using the mailbox and the delay in the same thread? I tried also bringing the delay before the for(;;) and it works.
Also, I can try to add more detail to the problem. The first thread send a mail of a certain type and then waits for a mail of another type; the thread in which I get the problem receive the mail go the first type and execute some code based on what it receive and then send the result as a mail of the second type; sometimes it is that it has to wait using osDelay and there it stop working but without going into any fault handler
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.