2017-12-17 11:14 PM
Hi All,
I'm using FreeRTOS and NUCLEO-F746ZG. Is there a way to get the size of the serial port buffer memory? The only way that I found is using register but I'm looking for a better solution.
@arg UART_FLAG_RXNE: Receive data register not empty flag
Can you propose some solution, please?
#free-rtos #nucleo2017-12-18 4:38 AM
There is no buffer provided by the peripheral/MCU, just RDR register. A buffer can be provided by using interrupt or DMA. See the
for information.2017-12-18 7:02 AM
In my case I use interrupts to read data from serial port. Let me give you little more information.
I have a problem with the incoming data. Each time the data size is different. We use RFID reader via serial port connection. Data is send to Nucleo board in different size each time.
How I can usebuffer from interrupts and get the size of the buffer?
What if I will use a FIFO struct linked to serial port, and every time there is a new byte, into ISR I will read byte and PUSH into FIFO.
After this, outside the ISR, 'higher level' application can check FIFO available data and POP from FIFO the received data.
For sure, FIFO struct have to be linked to a buffer large enough to save maximum length command received from serial port.
Is this a common way to manage receiving data from serial port
2017-12-18 8:07 AM
You would need to provide your own buffering and reporting methods. I typically use a software FIFO scheme, in extreme cases I use DMA bufferring where I understand the data stream properties, or must account for significant service latency.
Some of the newer parts (L4+, H7) have 8 or 16 word FIFOs, but the depth is not exposed.
2017-12-18 9:16 AM
Thanks for the reply. Do you know where I can find code snippet for this solution?
2017-12-19 6:16 AM
Sure, a FIFO can be used. It really just depends on your application, use-cases, etc.
For my application, I used a circular buffer. The ISR inserted into the buffer. An application task removed from the buffer. The circular buffer was sized to not overflow under 'normal' operation.
2017-12-19 12:12 PM
Can you show me code snippet or working example?
2017-12-19 12:29 PM
The use of a Ring Buffer - aka Circular Buffer or FIFO - is pretty much a universal standard when it comes to handling UARTs.
http://www.lmgtfy.com?q=microcontroller+UART+Ring+Buffer
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.