2025-02-18 11:45 PM
Hello everyone,
I'm experiencing an issue integrating the FP-AUD-AEC1 v1.2.0 library into my U5 microcontroller project and would appreciate some guidance on the echo cancellation algorithm's behavior.
My Setup:
The Issue: In my processAudioData function, I observed that the algorithm (specifically, the AcousticEC_Data_Input function) buffers data until it accumulates 128 bytes (with ECHO_BUFF set to 128). My expectation was that the algorithm would fill my output buffer with 8 bytes every 1 ms based on the 8 kHz sample rate—not in 128-byte (approximately 16 ms) segments.
Currently, the behavior appears as follows:
My Questions:
For additional context, my application involves two nodes, each equipped with a MEMS microphone and a speaker, communicating over CAN FD. Without the AEC enabled, the system works perfectly.
Any insights or recommendations would be greatly appreciated.
Thank you in advance for your help!
See below the code
// FS_AEC = 8000/1000
// int32_t i32_dataBuff[320] = {0}; // Input buffer: 320 bytes from MIC (24-bit data per sample)
// uint32_t u32_Buff_Output_Speaker[320] = {0}; // Output buffer: 320 bytes for speaker (24-bit data per sample)
// Processing 320 bytes to fill half of the SAI DMA buffer (40 ms of audio at 8 kHz)
#if ECHO_CANCELL
// Copy half of the audio buffer from the speaker acoustic queue
if (!FIFO_copyFromBuffer(&s_SpeakerAcusticQueue, &u32_Buff_Output_Speaker[0], AUDIO_BUFFER_SIZE / 2)) {
// Handle buffer copy failure if needed
}
// Calculate the number of 1 ms frames: 320 bytes / (8000 Hz / 1000) = 40 ms
u16_counter = _u16_audioSize / FS_AEC;
for (u16_counterAC = 0; u16_counterAC < u16_counter; u16_counterAC++) {
// Convert 24-bit MIC data to 16-bit PCM for echo cancellation
for (int u16_i = 0; u16_i < FS_AEC; ++u16_i) {
PCM_BufferAC[u16_i] = (int16_t)(i32_dataBuff[u16_counterAC * FS_AEC + u16_i] >> 8);
}
// Convert 24-bit speaker data to 16-bit PCM for echo cancellation
for (int u16_i = 0; u16_i < FS_AEC; ++u16_i) {
pAudio_out_8K[u16_i] = (int16_t)(u32_Buff_Output_Speaker[u16_counterAC * FS_AEC + u16_i] >> 8);
}
// Run acoustic echo cancellation (AEC) processing
if (AcousticEC_Data_Input(&PCM_BufferAC[0], pAudio_out_8K, &EchoOut[0], (AcousticEC_Handler_t *)&EchoHandlerInstance)) {
if (!AcousticEC_Process((AcousticEC_Handler_t *)&EchoHandlerInstance)) {
// Successfully processed: convert back to 24-bit format for SAI TX
for (int u16_i = 0; u16_i < FS_AEC; ++u16_i) {
i32_dataTemEco[u16_counterAC * FS_AEC + u16_i] = (int32_t)EchoOut[u16_i] << 8;
}
} else {
// This block should not be reached under normal conditions
Error_Handler();
}
} else {
// If AEC input fails, pass through the audio after restoring to 24-bit format
for (int u16_i = 0; u16_i < FS_AEC; ++u16_i) {
i32_dataTemEco[u16_counterAC * FS_AEC + u16_i] = (int32_t)EchoOut[u16_i] << 8;
}
}
}
// Send the processed 320-byte buffer to the speaker via SAI DMA
if (!FIFO_addToBuffer(&s_SpeakerQueue, (uint32_t *)i32_dataTemEco)) {
// Handle buffer overflow
Error_Handler();
}
// Transmit the same MIC data over CAN
memcpy(_u32_dataBuffCAN, i32_dataBuff, (_u16_audioSize) * sizeof(int32_t));
#else
2025-02-19 11:31 AM
Hello @eduarm
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Roger
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.