2021-12-15 5:00 AM
hello every one
We are developing a device with LwIP2.1.2 and FreeRTOS.
We used Comm Operator to test freemodbus and run an endurance tests with a polling modbus every 0.1 second.
but if we use both of them in same time(refresh the web and read data via modbus poll) it makes hard fault or Loop stuck(“tcp_input()�?�?�? tcp_send_fin()�?�?�? tcp_fasttmr()�?�?�? tcp_output()�?�?�? tcp_enqueue_flags()�?�?�? tcp_pcbs_sane()�?)!
Search for related problem data, but it will appear after the countermeasures.
https://savannah.nongnu.org/bugs/?59831
My English is not very well,If there's anything you haven't understood, please say so.
thanks for helping me
2021-12-17 3:47 PM
Did you read the topic you referred? Especially this post:
on 18 Jan 2021 08:51:00 PM UTC, comment #5:
Re comment #3:
Right. I would have closed this bug right away after reading the original post (sorry I keep finding no time for lwIP lately :-/). There's no way another task can run between those lines and modify lwIP variables. If it does, threading requirements are violated and the OP should read our docs.
Simon Goldschmidt <goldsimon>
And, if you are using ST's broken bloatware...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.