2025-04-08 3:45 AM - edited 2025-04-09 12:55 AM
Hi,
I'm trying to flash overt build in uart bootlader stm32 slave device. Here is my setup :
Master STM32F4 with tinyUSB
Slave STM32WLE5 device
Master and slave are connected together over uart. Master has control of boot0 and reset ligne of slave device.
Master UART2 PD5/PD6
Slave UART2 PA2/PA3
I'm able to put slave device into bootloader mode, but when I'm trying to connect with stm32cubeprogrammer over my usb I got NACK command from getId command
Here is the output of verbose mode cube programmer:
12:43:06:195 : UR connection mode is defined with the HWrst reset mode
12:43:06:257 : RTS low
12:43:06:257 : DTR low
12:43:06:277 : Serial Port cu.usbmodem123 is successfully opened.
12:43:06:277 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
12:43:06:277 : No Init bits value is : 0
12:43:06:277 : Sending init command:
12:43:06:277 : byte 0x7F sent successfully to target
12:43:06:277 : Wait ends after 1 loop, dataready = 1, delay = 5
12:43:06:277 : Received response from target: 0x79
12:43:06:277 : Activating device: OK
12:43:06:277 : Board : --
12:43:06:277 : Sending GetID command and its XOR:
12:43:06:278 : byte 0x02 sent successfully to target
12:43:06:278 : byte 0xFD sent successfully to target
12:43:06:278 : Wait ends after 1 loop, dataready = 1, delay = 6
12:43:06:278 : Received response from target: 0x1f
12:43:06:278 : Response received from device: NACK
12:43:06:278 : Error: GETID command not acknowledged!
12:43:06:278 : Reemission of GetID command
12:43:06:278 : Sending GetID command and its XOR:
12:43:06:278 : byte 0x02 sent successfully to target
12:43:06:278 : byte 0xFD sent successfully to target
12:43:06:278 : Wait ends after 1 loop, dataready = 1, delay = 7
12:43:06:278 : Received response from target: 0x1f
12:43:06:278 : Response received from device: NACK
12:43:06:278 : Error: GETID command not acknowledged!
12:43:06:278 : Reemission of GetID command
12:43:06:278 : Sending GetID command and its XOR:
12:43:06:278 : byte 0x02 sent successfully to target
12:43:06:278 : byte 0xFD sent successfully to target
12:43:06:278 : Wait ends after 1 loop, dataready = 1, delay = 6
12:43:06:278 : Received response from target: 0x1f
12:43:06:278 : Response received from device: NACK
12:43:06:278 : Error: GETID command not acknowledged!
12:43:06:278 : Chip ID: 0x0
12:43:06:278 : UART PORT CLOSE
Sometimes I'm able to get bootloader version and chip id and sometime not. My problem look realy similar to this post
If I try to use even parity my slave device never respond to 0x7F
EDIT: sometimes I can get chip id
15:45:23:537 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
15:45:23:537 : No Init bits value is : 0
15:45:23:538 : Sending init command:
15:45:23:538 : byte 0x7F sent successfully to target
15:45:23:538 : Wait ends after 1 loop, dataready = 1, delay = 5
15:45:23:538 : Received response from target: 0x79
15:45:23:538 : Activating device: OK
15:45:23:538 : Board : --
15:45:23:538 : Sending GetID command and its XOR:
15:45:23:538 : byte 0x02 sent successfully to target
15:45:23:538 : byte 0xFD sent successfully to target
15:45:23:538 : Wait ends after 1 loop, dataready = 1, delay = 7
15:45:23:538 : Received response from target: 0x1f
15:45:23:538 : Response received from device: NACK
15:45:23:538 : Error: GETID command not acknowledged!
15:45:23:538 : Reemission of GetID command
15:45:23:538 : Sending GetID command and its XOR:
15:45:23:538 : byte 0x02 sent successfully to target
15:45:23:538 : byte 0xFD sent successfully to target
15:45:23:538 : Wait ends after 1 loop, dataready = 1, delay = 6
15:45:23:538 : Received response from target: 0x79
15:45:23:538 : Received 4 data bytes from target : 0x01049779
15:45:23:538 : Chip ID: 0x497
15:45:23:538 : Sending Get command and its XOR:
15:45:23:538 : byte 0x00 sent successfully to target
15:45:23:539 : byte 0xFF sent successfully to target
15:45:23:539 : Wait ends after 1 loop, dataready = 0, delay = 1001
15:45:23:539 : Timeout error occured while waiting for acknowledgement.
15:45:23:539 : No response from target received
15:45:23:539 : Error: GET command not acknowledged!
15:45:23:539 : Reemission of Get command
15:45:23:539 : Sending Get command and its XOR:
15:45:23:539 : byte 0x00 sent successfully to target
15:45:23:539 : byte 0xFF sent successfully to target
15:45:23:539 : Wait ends after 1 loop, dataready = 1, delay = 5
15:45:23:539 : Received response from target: 0x1f
15:45:23:539 : Response received from device: NACK
15:45:23:539 : Error: GET command not acknowledged!
15:45:23:539 : Reemission of Get command
15:45:23:539 : Sending Get command and its XOR:
15:45:23:539 : byte 0x00 sent successfully to target
15:45:23:539 : byte 0xFF sent successfully to target
15:45:23:539 : Wait ends after 1 loop, dataready = 1, delay = 6
15:45:23:539 : Received response from target: 0x1f
15:45:23:539 : Response received from device: NACK
15:45:23:539 : Error: GET command not acknowledged!
15:45:23:539 : UART PORT CLOSE If I try to send command directly from serial terminal (coolterm for example) I have the same problem, first I send 0x7F my stm32wl5 respond 0x79
after send: 0x02, 0xFD, I only receive 0x79, 0x01, and sometime I receive all message.... Do we have to respect a precise timing between sending packets? bytes? I have try to send byte by byte same problem
Here is a small python script I used to test
import serial
import time
ser = serial.Serial('myCOM', baudrate=115200, timeout=1)
ser.write(b'\x7F')
ack = ser.read()
print(f"ACK 0x7F: {ack.hex()}")
time.sleep(0.5)
ser.write(b'\x02')
time.sleep(0.5)
ser.write(b'\xFD')
resp = ser.read(5)
print("Get ID:", resp.hex())First command always works, but for example second command 0x02,0xFD, if I send 2 bytes together I always got a NACK 0x1F ser.write(b'\x02\xFD'). //always NACK
But If I add a small sleep and send byte by byte 0x02 first and after sleep (0.5s like in my above script) 0xFD I got 0x79,0x01,0x79, why??
EDIT: it's look like as soon as I init my UART2 on my master stm32f4 device, I'm not able to connect with uart and stm32cubeprogrammer to my slave stm32. I've try to set parity NONE, EVEN, no change. It's only working if I don't init my UART2 on my master stm...
2025-04-09 9:48 AM
Hello @SBaro.11
@SBaro.11 wrote:
Hi,
I'm trying to flash overt build in uart bootlader stm32 slave device. Here is my setup :
Master STM32F4 with tinyUSBSlave STM32WLE5 device
Master and slave are connected together over uart. Master has control of boot0 and reset ligne of slave device.
Master UART2 PD5/PD6
Slave UART2 PA2/PA3
I'm able to put slave device into bootloader mode, but when I'm trying to connect with stm32cubeprogrammer over my usb I got NACK command from getId command
Could you explain your setup configuration with more details please?
2025-04-09 6:45 PM
My initial impression is that you are trying to use the master to update the slave using UART.
But then you mention stm32cubeprogrammer. So now it's unclear what you're trying to achieve with the master and stm32cubeprogrammer to update the slave?
Are you using the stm32cubeprogrammer to update the slave FW over UART using the DFU?
If so, what HW interface are you using and if that is connected to the same UART as the master?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.