STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N6 getting stuck in USB_CoreReset( )

I urgently need to get USB High Speed working on USB1 of the STM32N6570-DK. I have attached the .ioc file I am using.I am able to get the GPIO_IOToggle project working on the board. I am able to put breakpoints step through the code.I am using  STM32...

STM32F100C8T6B Bootloader issues

Posted on December 03, 2012 at 20:42I am trying to talk to the bootloader in the STM32F100 and having some issues. I can successfully send the 0x7F and get back a 0x79 ACK. Next when i send a Get Command i don't get any response. I am sending two by...

Resolved! Nucleo-U031R8 UART examples do not work?

Hi to all.I'm testing the Nucleo U031R8. To avoid the Package issue i switch also to the old package firmware version (1.0.0), but same error.The example is UART_HyperTerminal_IT  and i simple cloned (or compiled directly in the repository), then exe...

TheRaprus by Associate III
  • 2330 Views
  • 4 replies
  • 1 kudos

Resolved! Changing GPDMA Interrupts

Hello,I would like to enable and disable certain interrupts pertaining to the GPDMAs within my program at times. Particularly the transfer complete interrupt. I would assume that I should be able to simply change the register value with GPDMA2->C0CR ...

tw1_0-1743819810007.png
tw1 by Associate II
  • 1288 Views
  • 2 replies
  • 1 kudos

AzureRTOS Nx_TCP_Echo_Server on NUCLEO-H743ZI2

Hello everyone,I use the NUCLEO-H743ZI2 board in my project and previously, Before I've used the MBed OS - it works well on this board, just I need to maximize TCP transfer speed as well as QSPI. So I decided to try another RTOS. After reading forums...

Irek by Associate III
  • 12071 Views
  • 26 replies
  • 0 kudos

HAL_ADC_ConvHalfCpltCallback

I'm a beginner working with the STM32 Nucleo-L4R5ZI-P board and trying to set up ADC with DMA to sample an audio signal into a buffer. However, my DMA callback functions like HAL_ADC_ConvCpltCallback() and HAL_ADC_ConvHalfCpltCallback() are never bei...

stmuser by Associate
  • 1730 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G071 disco USBPD_Analyzer

Hi,I am trying to modify the USBPD_Analyer Demonstration to use a fixed PDO definition in the usbpd_pdo_defs.hEventually I would like to modify it to create a source slave as it is not available in the CubeMonitor-UCPD but to begin with I am just add...

aber by Associate
  • 946 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.