2025-10-06 10:42 AM - last edited on 2025-10-07 1:20 AM by Saket_Om
Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code
Hi everyone,
I’m trying to communicate with a Maxim DS2431 (1-Wire EEPROM) using an STM32F446RE MCU.
I can successfully generate the reset and sometimes detect a presence pulse, but when I send the Read ROM (0x33) command, the data I receive is always 0x00 for all 8 bytes.
I’m implementing the 1-Wire protocol manually (bit-banging) using a GPIO pin.
Below are the hardware details and what I’ve tried so far.
MCU: STM32F446RE @ 180 MHz
DS2431 powered at 3.3V (not parasitic)
1-Wire line connected to: GPIOA_PIN_0
Pull-up resistor: tried 2.2kΩ and 1.8
Is there anyone who has worked with DS2431 on STM32 before and can share experience, timing details, or working example code?
Thanks in advance :folded_hands:
Here is my 1-Wire read implementation:```c
/* USER CODE BEGIN Header */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#define DS2431_PORT GPIOA
#define DS2431_PIN GPIO_PIN_0
#include "string.h"
#include "stdio.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
extern UART_HandleTypeDef huart2;
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_TIM1_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void usDelay(uint16_t us)
{
__HAL_TIM_SET_COUNTER(&htim1, 0); // Counter'ı sıfırla
while (__HAL_TIM_GET_COUNTER(&htim1) < us); // Bekle
}
void OneWire_OutputLow(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = DS2431_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(DS2431_PORT, &GPIO_InitStruct);
HAL_GPIO_WritePin(DS2431_PORT, DS2431_PIN, GPIO_PIN_RESET);
}
void OneWire_Release(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = DS2431_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(DS2431_PORT, &GPIO_InitStruct);
}
uint8_t OneWire_ReadPin(void)
{
return HAL_GPIO_ReadPin(DS2431_PORT, DS2431_PIN);
}
/* -------------------------------------------------------------
* 1-WIRE RESET + PRESENCE DETECT
* ------------------------------------------------------------- */
uint8_t OneWire_Reset(void)
{
uint8_t presence = 1; // varsayılan: cihaz yok
// Hat LOW yap
OneWire_OutputLow();
usDelay(480); // Reset pulse
// Hat HIGH (release)
OneWire_Release();
usDelay(70); // Wait before presence check
// Presence okuyalım (0 = device present)
if (OneWire_ReadPin() == GPIO_PIN_RESET)
presence = 0;
usDelay(410); // Wait for end of timeslot
return presence; // 0 = presence detected, 1 = no device
}
/* -------------------------------------------------------------
* 1-WIRE WRITE BIT
* ------------------------------------------------------------- */
/* -------------------------------------------------------------
* 1-WIRE READ BIT
* ------------------------------------------------------------- */
uint8_t OneWire_ReadBit(void)
{
uint8_t bit = 0;
OneWire_OutputLow();
usDelay(6);
OneWire_Release();
usDelay(9);
bit = OneWire_ReadPin();
usDelay(55);
return bit;
}
uint8_t OneWire_ReadByte(void)
{
uint8_t data = 0;
for (int i = 0; i < 8; i++)
{
// Doğru bit pozisyonuna yerleştir
data >>= 1;
if (OneWire_ReadBit())
data |= 0x80;
// usDelay(1); // Bu satırı KALDIR - zaten ReadBit içinde delay var
}
return data;
}
void OneWire_WriteBit(uint8_t bit)
{
if (bit)
{
OneWire_OutputLow();
usDelay(6);
OneWire_Release();
usDelay(64);
}
else
{
OneWire_OutputLow();
usDelay(60);
OneWire_Release();
usDelay(10);
}
}
void OneWire_WriteByte(uint8_t data)
{
for (int i = 0; i < 8; i++)
{
OneWire_WriteBit(data & 0x01);
data >>= 1;
}
}
void OneWire_ReadROM(uint8_t *romData)
{
if (OneWire_Reset() == 0) // Presence kontrolü
{
OneWire_WriteByte(0x33); // Read ROM komutu
for (int i = 0; i < 8; i++)
{
romData[i] = OneWire_ReadByte();
}
}
else
{
}
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_TIM1_Init();
/* USER CODE BEGIN 2 */
uint8_t rom[8];
char buffer[100];
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while(1){
// HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
// usDelay(1000);
if (OneWire_Reset() == 0)
{
// Presence detected
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
OneWire_ReadROM(rom);
sprintf(buffer, "ROM = ");
HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY);
for (int i = 0; i < 8; i++)
{
sprintf(buffer, "%02X ", rom[i]);
HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY);
}
sprintf(buffer, "\r\n");
HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY);
}
else
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
// No device
}
}
// if (OneWire_Reset())
// {
// OneWire_ReadROM(rom);
//
// sprintf(buffer, "ROM = ");
// HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY);
//
// for (int i = 0; i < 8; i++)
// {
// sprintf(buffer, "%02X ", rom[i]);
// HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY);
// }
//
// sprintf(buffer, "\r\n");
// HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY);
// }
// else
// {
// char msg[] = "No presence detected.\r\n";
// HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
// }
//
// HAL_Delay(1000);
// }
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 180;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Activate the Over-Drive mode
*/
if (HAL_PWREx_EnableOverDrive() != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief TIM1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_TIM1_Init(void)
{
/* USER CODE BEGIN TIM1_Init 0 */
/* USER CODE END TIM1_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM1_Init 1 */
/* USER CODE END TIM1_Init 1 */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 100-1;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 0xffff-1;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM1_Init 2 */
HAL_TIM_Base_Start(&htim1);
/* USER CODE END TIM1_Init 2 */
}
/**
* @brief USART2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 9600;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
/*Configure GPIO pin : PA0 */
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PA5 */
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
```
2025-10-07 2:25 AM
Hello @farukke
Did you use an oscilloscope or logic analyser to verify whether the device is sending the correct data?
2025-10-07 2:47 AM - edited 2025-10-07 2:52 AM
@farukke wrote:I’m implementing the 1-Wire protocol manually (bit-banging) using a GPIO pin.
So how have you proved that your implementation is correct?
As @Saket_Om said, you need to use an oscilloscope to verify both timing and voltage levels.
@farukke wrote:I can successfully generate the reset and sometimes detect a presence pulse
Sounds very much like a timing issue...
@farukke wrote:Is there anyone who has worked with DS2431 on STM32 before and can share experience, timing details, or working example code?
Yes, there have been many previous threads on 1-WireTM - try a forum search; eg,
Rather than bit-banging, have you considered synthesising the timing using a UART or SPI?
PS:
@farukke wrote:a Maxim DS2431 (1-Wire EEPROM)
Note that it's now Analog Devices - they acquired Maxim 4 years ago:
https://www.analog.com/en/products/ds2431.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.