2022-07-21 11:01 AM
I am using the STM32G474RE and according to AN2606 Rev 55, it has a built-in bootloader in system memory. I set the option bytes such that the MCU boots from system memory and I will use the STM32Cubeprorammer CLI to program via USB.
In my application code, do I need to configure USB or will the built-in bootloader handle USB configuration on its own?
2022-10-03 8:45 AM
Hello,
>> Do I need to configure USB FS with the STM32CubeMX tool in the STM32CubeIDE for the built-in DFU bootloader to work?
No.
>> In my application code, do I need to configure USB or will the built-in bootloader handle USB configuration on its own?
You only need to configure the USB in the application code (maybe using CubeMX), if you use the USB from this application.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.