STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_ADC_ConvCpltCallback is called twice

I'm using an STM32F407, I want to use the falling edge of a PWM to trigger the ADC and then with the DMA move the data into a variable. The problem I have is that I am trying to check if the ADC is actually taking samples at the PWM frequency. I am t...

LSoll.1 by Associate II
  • 2795 Views
  • 2 replies
  • 0 kudos

Resolved! HAL SPI library: Does Master's single call to HAL_SPI_Transmit() always trigger Slave's both HAL_SPI_RxCpltCallback() and also HAL_SPI_TxCpltCallback() ?

I am coding STM32H743 MCU with CubeMX generated library.I have 1 SPI Master and 1 Slave. Both configured for a full SPI with both lines of Tx and Rx.Master is calling blocking HAL_SPI_Transmit() or HAL_SPI_Receive() but never simultaneous HAL_SPI_Tra...

eBirdman by Senior II
  • 2982 Views
  • 3 replies
  • 0 kudos

Writing own drivers vs HAL for professional project

Hi,firstly i apologise if this is in the wrong section as I'm asking more for technical advice than an answer for a specific technical question.First a bit of background:I'm a PhD student that is the sole engineer on a three year project that include...

CDyer.1 by Senior
  • 11375 Views
  • 28 replies
  • 4 kudos

How can I add "next_tag_part" to my function?

My string is too long to be inserted at once! And according LWIP manuals:LWIP_HTTPD_SSI_MULTIPART==1: SSI handler function is called with 2 more arguments indicating a counter for insert string that are too long to be inserted at once: the SSI handle...

DK.7 by Senior
  • 995 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G0B0: Prevent bootloader execution after RDP regression from level 1 to 0 and OBL causing mass erase and system reset

Hello,I would like to know how to prevent the execution of the on chip bootloader after a RDP regression from level 1 to level 0. After the necessary option byte load (OBL) a mass erase is done and the chip is reset and after the reset the bootloader...

DaMCU by Associate II
  • 5094 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.