2022-09-29 11:11 AM
Hello,
I am using the X-AZURE-CUBE example that integrates Azure RTOS with TF-M. I would like to define a function in the secure part to be called from the non-secure part. Following the SBSFU example I created a .c file in /Secure/Src, defined the .h file in Secure_nsclib and the function in the .c file has is defined with CMSE_NS_ENTRY. When I call this function from the non-secure part the microcontroller resets.
Thanks
2022-10-03 10:00 AM
Hi,
I defined a new secure service in the TFM_APP_ROT partition of the X-AZURE-CUBE example and I was able to call it correctly from the non-secure partition.
I defined a new secure partition, following the TF-M Adding Secure Partition guide, the files in the X-AZURE-CUBE example and updated the prebuild_secure.s script only when I try to run the code the device reboots continuously.
Checking the tfm_common_s.icf file, I noticed that the code for the secure partition I defined is missing. In the comments it says that the tfm_common_s.icf file is an autogenerated file, how is the tfm_common_s.icf file generated?
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.