2021-01-12 3:34 PM
Designing a board right now which has a STM32G072 to have two USB Type C ports, one sink and one DRP. First chip I looked at was the TCPP01-M12 - obviously it's the one on all the devboards. using it as a sink seems quite easy, though as a source or DRP seems more inconvenient (though not impossible) . Upon closer inspection of the datasheet I noticed a reference to two other devices, stated to be available in... q4 2020 in this, the only other mention on google. and for application in sources and DRPs. Any news on these devices? Seem quite handy, and would make good company with the TCPP01.
2021-01-13 6:52 AM
Hello,
The availability of TCPP02-M18 and TCPP03-M20 has been shifted to Q2 2021 (timing edited on Feb'21).
You may want to contact me directly by going on my profile and clicking on send message (kindly precise in your message that you authorize me to contact you directly) if you need more informations on these devices.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.