2020-11-07 6:27 AM
Continuous transmission of data of tx rate 500 samples per seconds(33 bytes per sample) using USB virtual com port(USB CDC).
USB mode - full speed
Transmit data to serial monitor using function CDC_Transmit_FS();
Received data on serial monitor is corrupted data, and this data corruption is not regular.
To solve this problem -
2020-11-09 6:09 AM
Not sure if this helps, but see https://community.st.com/s/question/0D50X00009XkhXw/usb-cdc-device-receive-fails-on-transmit
James
2020-11-09 9:48 PM
hi @James Murray
Problem is, data get corrupted when high speed data(16500 Bytes per second) transmission takes place.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.