2019-03-25 1:48 PM
Hi all,
I want to run an application to record audio from the microphone, as here is said:
https://www.youtube.com/watch?v=QIPQOnVablY
but my Cube doesn't have any options for DAC, there is only ADC1. For pin PA4, which should be DAC_OUTPUT, I have only ADC1_Input and GPIO_Analog available. Where did DAC disappear? I use eclipse with the newest Cube (5.1.0). Normally, in "Includes -> STMF4xx_HAL_Driver/Inc" there are the files for DAC (stm32f4xx_hal_dac_ex.h and stm32f4xx_hal_dac.h) but I haven't got them. Does anyone have the same problem? What can I do to add this files and use DAC?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.