2022-11-21 6:01 AM
I'm working on Over the Air and I have three components.
Bootloader in first two pages (using stm32f09x)
and applicaiton and then second application.
I'm unable to jump to application from bootloader for a specific reason.
I have one linker script, gave a build (app1) and made some modifications (app2).
How can I jump to application if the second slot application is having an address of reset handler which is pointing in the first location? (And let's say I add the offset of the app1 size, am I sure that the reset handler stays in the exact same location everytime i give a build)?
Help me out here. My master thesis time is running out.
One solution I am implementing is two use two binary images and upload to the cloud but i think this is a patchy idea, I was something solid if you have one.
Thanks in advance.
2022-11-21 7:01 AM
f0 doesnt have a vector table offset, you need to do it yourself, at the beginning of each app the first thing you should do is realocate your vector table to RAM.
>>My master thesis time is running out.
If you need some help with this hit me up
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.