STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unused pins to ground and bootloader question

Hello,I would like to put many pins on my UFBGA STM32 to ground, and configure in software as input or even better output( must be done correctly first time )But now I am wondering, if I am planning to BOOT processor with BOOT pin high, and use UART ...

0693W00000Lzai0QAB.png
Linas L by Senior II
  • 1541 Views
  • 2 replies
  • 1 kudos

Resolved! missing stm32f4xx_hal_uart.h in STM32F4xx_HAL_Driver

I recently go the 32F413HDISCOVERY board and downloaded the projects and examples to a local folder and imported it all of it into STM32CubeIDE.In the STM32CubeIDE I was able to open and modify the Test_001 project and blink LED2 and LED3. Next, I wa...

IMate.1 by Associate II
  • 6177 Views
  • 3 replies
  • 0 kudos

HAL QSPI AUTOPOLLING SUPPORT 4LINES?

I have read many samples in cube h7 github repository, and I have seen any hal autoplling example consulting status registers in 4 lines mode operation. It is supported? I am using STM32H750 with cube h7 1.10.0.

JCuna.1 by Senior
  • 2469 Views
  • 4 replies
  • 0 kudos

STM32G0B1KE System Bootloader Mode Entry

Hello ST Community,We are using STM32G0B1KE MCU in our project. The MCU firmware will be flashed from the Processor via the I2C interface between the processor and MCU.As per AN2606, we have tried to activate pattern 11, but the system bootloader cou...

Malik1 by Associate
  • 2016 Views
  • 3 replies
  • 0 kudos

Is there any Real time timer in stm32

Hello Everyone,I am using STM32H7 series of microcontroller and in Atmel SAM E70/S70 series of microcontroller they give Real time timer feature,please refer below datasheet for Atmel Section 28 and page number 229.https://ww1.microchip.com/downloads...

Resolved! Programming using I2C

Hello all, I have a design that is designed with a STM32. The SWDIO pin and SWCLK pin are pogo test points and difficult to solder wires to connect to the ST link programmer. The design has the BOOT0 pin pulled up to VDD. The I2C lines are the only ...

0693W00000Lz7SDQAZ.png
VThan.2 by Associate III
  • 4023 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.