2021-03-05 6:16 AM
Hello,
I'm trying to change the HID report to x and y have more accuracy (If i', not wrong, windows drivers accept this without any proprietary driver).
My HID mouse report in usbd_hid.c is:
__ALIGN_BEGIN static uint8_t HID_MOUSE_ReportDesc[HID_MOUSE_REPORT_DESC_SIZE] __ALIGN_END =
{
0x05, 0x01, // Usage Page (Generic Desktop Ctrls)
0x09, 0x02, // Usage (Mouse)
0xA1, 0x01, // Collection (Application)
0x09, 0x01, // Usage (Pointer)
0xA1, 0x00, // Collection (Physical)
0x05, 0x09, // Usage Page (Button)
0x19, 0x01, // Usage Minimum (0x01)
0x29, 0x05, // Usage Maximum (0x05)
0x15, 0x00, // Logical Minimum (0)
0x25, 0x01, // Logical Maximum (1)
0x95, 0x05, // Report Count (5)
0x75, 0x01, // Report Size (1)
0x81, 0x02, // Input (Data,Var,Abs,No Wrap,Linear,Preferred State,No Null Position)
0x95, 0x03, // Report Count (3)
0x75, 0x01, // Report Size (1)
0x81, 0x01, // Input (Const,Array,Abs,No Wrap,Linear,Preferred State,No Null Position)
0x05, 0x01, // Usage Page (Generic Desktop Ctrls)
0x09, 0x30, // Usage (X)
0x09, 0x31, // Usage (Y)
0x16,0x01,0x80, // Logical Minimum (-32767)
0x26,0xFF,0x7F, // Logical Maximum (32767)
0x75, 0x016, // Report Size (8)
0x95, 0x02, // Report Count (2)
0x81, 0x06, // Input (Data,Var,Rel,No Wrap,Linear,Preferred State,No Null Position)
0x09, 0x38, // Usage (Wheel)
0x15, 0x81, // Logical Minimum (-127)
0x25, 0x7F, // Logical Maximum (127)
0x75, 0x08, // Report Size (8)
0x95, 0x01, // Report Count (1)
0x81, 0x06, // Input (Data,Var,Rel,No Wrap,Linear,Preferred State,No Null Position)
0xC0, // End Collection
0x09, 0x3C, // Usage (Motion Wakeup)
0x05, 0xFF, // Usage Page (Reserved 0xFF)
0x09, 0x01, // Usage (0x01)
0x15, 0x00, // Logical Minimum (0)
0x25, 0x01, // Logical Maximum (1)
0x75, 0x01, // Report Size (1)
0x95, 0x02, // Report Count (2)
0xB1, 0x22, // Feature (Data,Var,Abs,No Wrap,Linear,No Preferred State,No Null Position,Non-volatile)
0x75, 0x06, // Report Size (6)
0x95, 0x01, // Report Count (1)
0xB1, 0x01, // Feature (Const,Array,Abs,No Wrap,Linear,Preferred State,No Null Position,Non-volatile)
0xC0, // End Collection
// 86 bytes
};i changed the lines:
And I changed in usbd_hid:
#define HID_EPIN_ADDR 0x81U
#define HID_EPIN_SIZE 0x06U
#define USB_HID_CONFIG_DESC_SIZ 34U
#define USB_HID_DESC_SIZ 9U
#define HID_MOUSE_REPORT_DESC_SIZE 86U
#define HID_DESCRIPTOR_TYPE 0x21U
#define HID_REPORT_DESC 0x22U
#ifndef HID_HS_BINTERVAL
#define HID_HS_BINTERVAL 0x07U
#endif /* HID_HS_BINTERVAL */
#ifndef HID_FS_BINTERVAL
#define HID_FS_BINTERVAL 0x0AU
#endif /* HID_FS_BINTERVAL */
#define HID_REQ_SET_PROTOCOL 0x0BU
#define HID_REQ_GET_PROTOCOL 0x03U
#define HID_REQ_SET_IDLE 0x0AU
#define HID_REQ_GET_IDLE 0x02U
#define HID_REQ_SET_REPORT 0x09U
#define HID_REQ_GET_REPORT 0x01UWhen i try to connect to PC I have the following error:
I have to change anything else?
Where am I wrong?
Thanks in advance
2021-03-05 7:36 AM
Error in line 24.
> 0x75, 0x016,
You want probably report size 16 (decimal), count 2
-- pa
2021-03-08 12:48 AM
Hello,
Thanks for the answered, you're agree.
Now with this change i don't have the descriptor problem, but the PC didn't recognize my 'mouse'. This descriptor is compatible with HID? Or with this change i will have to develop a driver for windows?
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.