2022-10-24 6:25 AM
I have a GPS module and I use it by connecting it to my computer via USB.
I also want a CAN bus output.
Can I use the STM32F730R8T6 processor?
How can I introduce the information from the USB to the STM32 processor? Which pins should I use?
After doing this I also need to get a CAN bus output.
Can you help me?
2022-10-24 10:01 AM
First, get familiar with USB CDC or HID class - both are supported by CubeMX, choose the one which suits you best.
2022-10-24 11:48 AM
You can see if this video will get you started https://www.youtube.com/watch?v=oe5JmYYAZy0
It shows how to set the STM32 as a Custom HID device and also use CAN bus.
2022-10-25 3:27 AM
STM32F730R8T6 is a bit overkill but yes,
MIND the extra transceiver needed : almost everyone forgets they need the canbus transceiver IC when starting with canbus
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.