STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

B-L462E-CELL1 Developer Support Request

Hi there,I am trying to explore IoT options with the B-L462E-CELL1 discovery kit (STM32L462RE mcu). I was hoping for a software environment that I could use as a springboard to start working with this device, but I have not been able to find one.I ha...

LPuck.1 by Associate
  • 1604 Views
  • 1 replies
  • 1 kudos

Is there a socket allocation problem with X-CUBE-CELLULAR V7.0 using Azure RTOS and the STM32L462RE discovery kit Cellular IOT board?

In this loop the mqtt client is created, connected and as long as the mqtt server/broker is up, the client continues processing messages. But when the remote mqtt server/broker is manually shut down, and after the timeout expires, nxd_mqtt_client_c...

JVand.12 by Associate II
  • 1158 Views
  • 0 replies
  • 0 kudos

Resolved! How to switch the DMA buffer in HAL_SPI_Transmit_DMA

While output data from DMA to SPI it should be able to use two buffers. One for the current transfer, one to write data.But how do I switch between the buffers?#define BUFFER_SIZE 10 uint8_t txBuffer[BUFFER_SIZE + BUFFER_SIZE]; HAL_SPI_Transmit_DMA(&...

Wechmarer by Associate II
  • 1612 Views
  • 1 replies
  • 0 kudos

I2C bootloader not working on stm32G030

we are using stm32G030, we need to update firmware using I2C, we are using st-link v3 and we connected (SCL,SDA,GND), opened cube programmer to update firmware we selected I2C and and given i2c address as 0xAD/0xAC but we are getting I2C_BRG_ERR,wha...

0693W00000Kc64PQAR.png 0693W00000Kc64tQAB.png
pGami.1 by Associate
  • 1720 Views
  • 1 replies
  • 0 kudos

f4 lwip doesn't work in updated latest

I used 1.7version now i renew my project couple of days agoI guess problem with 1) LWIP/TARGET/ethernetif.c, 2) LWIP/TARGET/ethernetif.h, 3) LWIP/TARGET/lwipopts.h4) stm32f4xx_hal_eth.c5) stm32f4xx_hal_eth.hI got searched lwip thread i think new ve...

SKim.1761 by Associate III
  • 1073 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.