2021-11-19 1:02 AM
Hello,
there is a race condition in the function SD_read() in the template file used by CubeMX when using FATFS with DMA template (sd_diskio_dma_template_bspv1.c).
if(BSP_SD_ReadBlocks_DMA((uint32_t*)buff,
(uint32_t) (sector),
count) == MSD_OK)
{
ReadStatus = 0;The variable ReadStatus should be set to zero BEFORE the call to BSP_SD_ReadBlocks_DMA(), as it is already the case in the BSP V2 template (sd_diskio_dma_template_bspv2.c) and in the examples using FATFS and SD DMA (e.g. Projects\STM32F412G-Discovery\Applications\USB_Host\AUDIO_Standalone\Src\sd_diskio_dma.c).
2021-11-29 7:10 AM
Good catch @Grann !
I'll report this limitation to our development team who will take care to provide a fix.
Internal ticket number: 118428 (PS: This is an internal tracking number and is not accessible or usable by customers).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-21 10:29 AM
Any updates on when this will be fixed?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.