2026-03-04 4:32 AM - last edited on 2026-03-04 4:57 AM by mƎALLEm
Hi ST Community,
I'm wondering if there's a sample project for a UART Bootloader for the NUCLEO-H755ZI-Q series.
Thanks for your support
Solved! Go to Solution.
2026-03-04 5:02 AM - edited 2026-03-04 5:03 AM
+
AN3155 «How to use USART protocol in bootloader on STM32 MCUs »
2026-03-04 4:36 AM - edited 2026-03-04 4:37 AM
Do you mean a custom bootloader over UART?
PS: I don’t see why posting this question in CubeIDE forum board!
2026-03-04 4:46 AM
not customized but a minimal example of bootloader operation via uart (.bin file)
2026-03-04 4:52 AM
I think the question was "custom bootloader" vs the System bootloader in ROM ?
So custom bootloader:
System bootloader:
2026-03-04 4:56 AM - edited 2026-04-01 8:34 AM
A question on a minimal example of « something » needs to be posted in Embedded software forum board. CubeIDE forum is only dedicated to raise question/issues on the tool or to suggest an enhancement. This post will be moved then.
Thank you.
2026-03-04 5:02 AM - edited 2026-03-04 5:03 AM
+
AN3155 «How to use USART protocol in bootloader on STM32 MCUs »
2026-03-04 5:11 AM
Thanks for the documentation, I meant some examples already developed for that series
2026-03-04 5:21 AM
Why don’t use the ST bootloader like indicated by the application notes provided above?
2026-03-04 6:20 PM
https://github.com/STMicroelectronics/stm32-mw-openbl
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.