STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi i'm working on Nucleo-l073rz board to bring up sd card and fatfs using spi interface for data logging application.

I am testing the above setup using an transcend micro sd card adapter with 16GB sd card.I have no response from the sd card , i have used 32MHz clock with a spi baud rate 8MBits/s.i have used drivers from  STM32Cube_FW_L0_V1.11.2\Drivers\BSP\Adafruit...

svii by Associate III
  • 1383 Views
  • 2 replies
  • 0 kudos

So are there successful implementation of

I'm using STM32F767ZI MCU based Nucleo -F767ZI development board, which is supporting Ethernet communication protocol and so on. I have a motor driver which is supporting the EtherCAT communication interface, and I want to interface that motor driver...

AMish.5 by Associate
  • 698 Views
  • 0 replies
  • 0 kudos

STM32F429 USB problem when Vector Relocated

Hi all,I am using STM32F429AG for one of our project. When i use vector table at its default position USB virtual com port works perfectly. However, when i relocate the Vector table, my windows pc gives error that the USB device is malfunctioning. Ot...

SAkta.1 by Associate
  • 1914 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F767 + CMSIS DSP + Keil = Error.

Im trying to use rftt_q15 from CMSIS DSP libraries on my STM32F767ZiThe following error I get is quite strange. it says #error "Define according the used Cortex core ARM_MATH_CM7, ARM_MATH_CM4, ARM_MATH_CM3, ARM_MATH_CM0PLUS, ARM_MATH_CM0, ARM_MATH_A...

hashtala by Associate II
  • 4650 Views
  • 4 replies
  • 0 kudos

STM32G4 ADC12_Common Register cannot be written

Hi! I am trying to set ADC pre-scaler of my STM32G431KB however no matter what I do it never changes from 0x0.I can setup ADC1 register without a problem but when it comes to ADC12_Common register nothing seems to be configurable. Below there is my A...

LLOLO.1 by Associate II
  • 2096 Views
  • 6 replies
  • 0 kudos
DCull.1 by Associate
  • 1785 Views
  • 1 replies
  • 0 kudos

SAI - get best clock accuracy

Hi :) This is related to my other post (https://community.st.com/s/question/0D53W00000EcBvNSAV/sai-no-signal-on-mclk-pin) but I thought it would be more organised to make two posts since the question is different.How do I get the best audio clock acc...

0693W000002lgZ0QAI.png
SLasn.1 by Senior
  • 5833 Views
  • 11 replies
  • 0 kudos

USB device library. CDC behavior at USB host reset

Hi all,We are using the en.stm32_f105-07_f2_f4_usb-host-device_lib_2.2.0 library for CDC functionality. Our STM32 ist USB device connected with host. Everything working fine till the host gets HW reset. Then sometimes after host booted again the STM3...

SVely.1 by Associate
  • 1062 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.