STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USBPD message sequence issue.

Hi STteam,@brief : We are working PD source solution(i.e. 60Watt (20V @ 3A max)) using STM32G081RBT6. We are taking USB-PD_Provider_1port as an Base reference project.@Reference : I have gone through each and every line of UM2552 reference manual I f...

HGorl.1 by Associate II
  • 1259 Views
  • 1 replies
  • 0 kudos

Issues with SD Card when waiting for SD Card Ready

Hi everybody,I've got an STM32H743XI and use the Cube V1.3.2 Firmware for an project for my master thesis.To this controller I have connected a SD Card with the SDMMC controller using the 4 bit bus. I also use FreeRtos and don't want a blocking read ...

maxmax1 by Associate
  • 1843 Views
  • 2 replies
  • 1 kudos

Resolved! Where are peripherals initialized?

I am implementing a USBPD application, using the NUCLEO-G474RE example of x-cube-usbpdm1 (it is called TCPP01_Consumer).The example works fine, but I am a bit confused as to where all the peripherals are initalized. The MX init functions are generate...

FGeig.1 by Associate III
  • 2056 Views
  • 2 replies
  • 0 kudos

Resolved! Ethernet interrupt can't be triggered

Hi,​I'm working on STM32F407 board, and trying to enable ethernet with ThreadX + Netxduo. I referred several successful cases for the porting, and did everything I can do, but it's not pingable at all. I did some debug, and found the ETH_IRQHandler i...

XLei.1 by Associate II
  • 2025 Views
  • 1 replies
  • 0 kudos

Uart Interrupt in FreeRTOS ?

I want implement FreeRTOS in my project. I created 2 tasks osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128); defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL); osThreadDef(Task1, Task1, osPriorityIdle, 0, 128); Task1...

0693W000006F5JvQAK.png
srikanth by Associate III
  • 1303 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.