STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USB High Speed read SD card only 1 MB/s

Hello!I am using STM32F427VGT with USB3300 as USB high speed device mass storage class. I want to read data from SD card to a PC and I am only able to get transfer speed about 1 MB/s. What is the real maximum read speed that I can get with this hardw...

dzikos by Associate II
  • 2147 Views
  • 2 replies
  • 0 kudos

UCPD Sink demo on B-G474E does not select PDO

HiI am using a UCPD demo of STM32G4 B-G474 (USB-PD_Consumer_1port) but it does not allow me to select any of the Source PDOs. The sink can see the capabilities of the source but not select any. Can you help me with this? I am using STM32CubeIDE and ...

0693W000006FNs5QAG.png 0693W000006FNsFQAW.png 0693W000006FNsKQAW.png
MPaz.1 by Associate
  • 1140 Views
  • 1 replies
  • 0 kudos

In Application Program to STM32H750 .

hi I am using STM32H750 MCU in my custom board. I want program by using IAP(in application program) . I wrote main boot code size of 19k and (flash size I took 32k from IROM1:0x08000000 - 0x8000) , I programmed to application address is 0x0800800...

srikanth by Associate III
  • 1247 Views
  • 1 replies
  • 0 kudos

Hi, I try to communication with two stm32f4 via CAN bus. the first board (which transmit the message) as can1 and the second (which receive the message) as can2. I'm using the new HAL_CAN function.

In polling mode, HAL_CAN_AddTxMessage() returns HAL_OK, but HAL_CAN_GetRxMessage() returns HAL_CAN_ERROR_PARAM. In interrupt mode, the function HAL_CAN_RxFifo0MsgPendingCallback() never has been called (CAN1_RX0_IRQHandler not been called). Also HAL...

AS.5 by Associate II
  • 3803 Views
  • 5 replies
  • 0 kudos

Windows Driver/INF files for ECM

Hi there,Windows does not contain a default ECM driver like Linux does. I was wondering if there was any intention providing a Windows driver for the ECM middleware that is in the framework? We have to work with specific Android phones, which do no...

JKaz.1 by Associate III
  • 801 Views
  • 1 replies
  • 0 kudos

PDM2PCM Library will not link.

Hi.I'm working on a STM32F4-Discovery board, and I'm having trouble linking the PDM2PCM Library into my project. I have run the example project located in the STM32F4-Discovery folder called "Audio_playback_and_record" and it works fine.I have copied...

0690X00000Aq089QAB.jpg
mbmail4 by Associate II
  • 2439 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.