STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ARM based device with EMIF

Hello,I'm looking for an ARM based MCU or MPU that has the following peripherals:Parallel External Memory InterfaceI2CSPIUARTMII (for ethernet management)Please suggest whether ST offers such a device.

skon.1 by Senior
  • 1639 Views
  • 2 replies
  • 0 kudos

SM32G071xB Configure option bytes from UART

I have Nucleo-G071RB board when I flash the Option Bytes to load from system memory (Bootloader) via ST-link it works with just reset and I can access the Bootloader,But when I try to edit the Option Bytes via UART, I need to power off the board and ...

Resolved! Run or Debug sample_threadx sample from Azure_RTOS_6.1_STM32F746G-DISCO_STM32CubeIDE_Samples_2020_10_10.zip

In October 2020 Microsoft released sample applications to try out Azure on some reference boards. One of them is STM32F746G-DISCO. Downloaded Azure_RTOS_6.1_STM32F746G-DISCO_STM32CubeIDE_Samples_2020_10_10.zip from https://github.com/azure-rtos/sampl...

VSubb.1 by Associate
  • 1170 Views
  • 1 replies
  • 0 kudos

How does one install en.stm32cubeh7_v1-8-0 Software?

File downloaded, and appears to have unzipped fine.No obvious Executable File is present, to install on Windows 10.UM2204 "Getting started with STM32CubeH7 for STM32H7 Series" does not mention Installation, which would be really helpful, for getting ...

ACole.1 by Associate II
  • 3678 Views
  • 8 replies
  • 0 kudos

Resolved! STM32F746-DISCO audio delay line implementation problem.

I have audio pass-through working project for STM32F746/769 DISCO module, where block of 4 samples (2 left and 2 right channel ones) from input are passed to output chanell DMA buffer.My delay line implementation is as follows:#define BUFF_SIZE 4 #de...

RRumi by Associate II
  • 4770 Views
  • 9 replies
  • 0 kudos

STcube MX code issue

Hi Team,Facing some issues on belowHAL Delay goes into infinite loop or the program stops there only (Inside the "IF" condition)"IF" Condition works, data transfer works, but Toggling of pin, or any action with Delay command is not working Upon going...

SS_135 by Associate II
  • 940 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.